SimpleLink CC3120/CC3220 Host Driver
Version 2.0.1.15
Simplifies the implementation of Internet connectivity
|
Data Fields | |
_u8 | TokenValueLen |
_u8 | TokenNameLen |
_u8 | TokenName [SL_NETAPP_MAX_TOKEN_NAME_LEN] |
_u16 | Padd |
Definition at line 936 of file protocol.h.
_u16 Padd |
Definition at line 941 of file protocol.h.
_u8 TokenName[SL_NETAPP_MAX_TOKEN_NAME_LEN] |
Definition at line 940 of file protocol.h.
_u8 TokenNameLen |
Definition at line 939 of file protocol.h.
_u8 TokenValueLen |
Definition at line 938 of file protocol.h.