SimpleLink CC3120/CC3220 Host Driver
Version 2.0.1.22
Simplifies the implementation of Internet connectivity
|
Data Fields | |
_i16 | LenOrPadding |
_u8 | Sd |
_u8 | FamilyAndFlags |
_u16 | Port |
_u16 | PaddingOrAddr |
_u32 | Address [4] |
Definition at line 830 of file protocol.h.
_u32 Address[4] |
Definition at line 837 of file protocol.h.
_u8 FamilyAndFlags |
Definition at line 834 of file protocol.h.
_i16 LenOrPadding |
Definition at line 832 of file protocol.h.
_u16 PaddingOrAddr |
Definition at line 836 of file protocol.h.
_u16 Port |
Definition at line 835 of file protocol.h.
_u8 Sd |
Definition at line 833 of file protocol.h.