SimpleLink CC3120/CC3220 Host Driver
Version 2.0.1.22
Simplifies the implementation of Internet connectivity
|
Data Fields | |
_u8 | Ip [4] |
_u8 | IpMask [4] |
_u8 | IpGateway [4] |
_u8 | IpDnsServer [4] |
_u8 | IpStart [4] |
_u8 | IpEnd [4] |
Definition at line 716 of file protocol.h.
_u8 Ip[4] |
Definition at line 718 of file protocol.h.
_u8 IpDnsServer[4] |
Definition at line 721 of file protocol.h.
_u8 IpEnd[4] |
Definition at line 723 of file protocol.h.
_u8 IpGateway[4] |
Definition at line 720 of file protocol.h.
_u8 IpMask[4] |
Definition at line 719 of file protocol.h.
_u8 IpStart[4] |
Definition at line 722 of file protocol.h.