SimpleLink CC3120/CC3220 Host Driver
Version 2.0.1.22
Simplifies the implementation of Internet connectivity
|
Data Fields | |
_u16 | Status |
_u16 | Padding |
_u32 | Ip0 |
_u32 | Ip1 |
_u32 | Ip2 |
_u32 | Ip3 |
Definition at line 1029 of file protocol.h.
_u32 Ip0 |
Definition at line 1033 of file protocol.h.
_u32 Ip1 |
Definition at line 1034 of file protocol.h.
_u32 Ip2 |
Definition at line 1035 of file protocol.h.
_u32 Ip3 |
Definition at line 1036 of file protocol.h.
_u16 Padding |
Definition at line 1032 of file protocol.h.
_u16 Status |
Definition at line 1031 of file protocol.h.