SimpleLink CC3120/CC3220 Host Driver
Version 2.0.1.22
Simplifies the implementation of Internet connectivity
|
Data Fields | |
_u8 | TokenValueLen |
_u8 | TokenNameLen |
_u8 | TokenName [SL_NETAPP_MAX_TOKEN_NAME_LEN] |
_u16 | Padd |
Definition at line 962 of file protocol.h.
_u16 Padd |
Definition at line 967 of file protocol.h.
_u8 TokenName[SL_NETAPP_MAX_TOKEN_NAME_LEN] |
Definition at line 966 of file protocol.h.
_u8 TokenNameLen |
Definition at line 965 of file protocol.h.
_u8 TokenValueLen |
Definition at line 964 of file protocol.h.