#include <SDSPICC32XX.h>
§ baseAddr
uint32_t SDSPICC32XX_HWAttrsV1::baseAddr |
< SPI Peripheral base address
§ spiPRCM
uint32_t SDSPICC32XX_HWAttrsV1::spiPRCM |
SPI PRCM peripheral number GSPI CLK pin assignment
§ clkPin
uint32_t SDSPICC32XX_HWAttrsV1::clkPin |
GSPI MOSI pin assignment & GPIO encoding when using MOSI as GPIO
§ mosiPin
uint32_t SDSPICC32XX_HWAttrsV1::mosiPin |
§ misoPin
uint32_t SDSPICC32XX_HWAttrsV1::misoPin |
CS pin assignment & GPIO encoding for pin use as GPIO
§ csPin
uint32_t SDSPICC32XX_HWAttrsV1::csPin |
The documentation for this struct was generated from the following file: