SDHostCC32XX Object. More...
#include <SDHostCC32XX.h>
Data Fields | |
uint_fast32_t | rca |
const uint_fast32_t * | writeBuf |
volatile uint_fast32_t | writeSecCount |
uint_fast32_t * | readBuf |
volatile uint_fast32_t | readSecCount |
SemaphoreP_Handle | cmdSem |
HwiP_Handle | hwiHandle |
unsigned int | powerMgrId |
Power_NotifyObj | postNotify |
PowerCC32XX_ParkState | prevParkCLK |
uint16_t | clkPin |
UDMACC32XX_Handle | dmaHandle |
volatile int_fast8_t | stat |
bool | isOpen |
SD_CardType | cardType |
SDHostCC32XX Object.
The application must not access any member variables of this structure!
uint_fast32_t SDHostCC32XX_Object::rca |
const uint_fast32_t* SDHostCC32XX_Object::writeBuf |
volatile uint_fast32_t SDHostCC32XX_Object::writeSecCount |
uint_fast32_t* SDHostCC32XX_Object::readBuf |
volatile uint_fast32_t SDHostCC32XX_Object::readSecCount |
SemaphoreP_Handle SDHostCC32XX_Object::cmdSem |
HwiP_Handle SDHostCC32XX_Object::hwiHandle |
unsigned int SDHostCC32XX_Object::powerMgrId |
Power_NotifyObj SDHostCC32XX_Object::postNotify |
PowerCC32XX_ParkState SDHostCC32XX_Object::prevParkCLK |
uint16_t SDHostCC32XX_Object::clkPin |
UDMACC32XX_Handle SDHostCC32XX_Object::dmaHandle |
volatile int_fast8_t SDHostCC32XX_Object::stat |
bool SDHostCC32XX_Object::isOpen |
SD_CardType SDHostCC32XX_Object::cardType |