73 #ifndef ti_drivers_sd_SDHostCC32XX__include 74 #define ti_drivers_sd_SDHostCC32XX__include 83 #include <ti/drivers/dpl/HwiP.h> 84 #include <ti/drivers/dpl/SemaphoreP.h> 89 #define SDHostCC32XX_PIN_06_SDCARD_DATA 0x0805 90 #define SDHostCC32XX_PIN_07_SDCARD_CLK 0x0806 91 #define SDHostCC32XX_PIN_08_SDCARD_CMD 0x0807 92 #define SDHostCC32XX_PIN_01_SDCARD_CLK 0x0600 93 #define SDHostCC32XX_PIN_02_SDCARD_CMD 0x0601 94 #define SDHostCC32XX_PIN_64_SDCARD_DATA 0x063f volatile int_fast8_t stat
Definition: SDHostCC32XX.h:196
SemaphoreP_Handle cmdSem
Definition: SDHostCC32XX.h:180
struct SDHostCC32XX_HWAttrsV1 SDHostCC32XX_HWAttrsV1
uint32_t clkPin
Definition: SDHostCC32XX.h:157
uint_fast32_t baseAddr
Definition: SDHostCC32XX.h:142
int_fast32_t intPriority
Definition: SDHostCC32XX.h:139
Power_NotifyObj postNotify
Definition: SDHostCC32XX.h:188
uint_fast32_t clkRate
Definition: SDHostCC32XX.h:136
SDHostCC32XX Object.
Definition: SDHostCC32XX.h:165
Power notify object structure.
Definition: Power.h:113
uint32_t dataPin
Definition: SDHostCC32XX.h:151
volatile uint_fast32_t writeSecCount
Definition: SDHostCC32XX.h:171
SD_CardType cardType
Definition: SDHostCC32XX.h:200
uDMA driver implementation for CC32XX.
bool isOpen
Definition: SDHostCC32XX.h:198
UDMACC32XX Global configuration.
Definition: UDMACC32XX.h:135
Power manager interface for the CC32XX.
uint32_t cmdPin
Definition: SDHostCC32XX.h:154
unsigned long txChIdx
Definition: SDHostCC32XX.h:148
struct SDHostCC32XX_Object SDHostCC32XX_Object
SDHostCC32XX Object.
UDMACC32XX_Handle dmaHandle
Definition: SDHostCC32XX.h:194
HwiP_Handle hwiHandle
Definition: SDHostCC32XX.h:184
PowerCC32XX_ParkState prevParkCLK
Definition: SDHostCC32XX.h:190
uint16_t clkPin
Definition: SDHostCC32XX.h:192
uint_fast32_t rca
Definition: SDHostCC32XX.h:167
The definition of a SD function table that contains the required set of functions to control a specif...
Definition: SD.h:266
uint_fast32_t * readBuf
Definition: SDHostCC32XX.h:173
enum SD_CardType_ SD_CardType
SD Card type inserted.
volatile uint_fast32_t readSecCount
Definition: SDHostCC32XX.h:175
unsigned long rxChIdx
Definition: SDHostCC32XX.h:145
const SD_FxnTable sdHostCC32XX_fxnTable
Definition: SDHostCC32XX.h:134
unsigned int powerMgrId
Definition: SDHostCC32XX.h:186
const uint_fast32_t * writeBuf
Definition: SDHostCC32XX.h:169
PowerCC32XX_ParkState
Enumeration of states a pin can be parked in.
Definition: PowerCC32XX.h:385