EDMA3 Driver Object (HW Specific) Maintenance structure. More...
#include <edma3.h>
Data Fields | |
uint32_t | phyCtrllerInstId |
EDMA3_DRV_ObjState | state |
uint32_t | numOpens |
EDMA3_DRV_GblConfigParams | gblCfgParams |
Init-time Configuration structure for EDMA3 controller, to provide Global SoC specific Information. |
EDMA3 Driver Object (HW Specific) Maintenance structure.
Used to maintain information of the EDMA3 HW configuration thoughout the lifetime of the EDMA3 Driver Object, one for each EDMA3 hardware instance.
uint32_t EDMA3_DRV_Object::phyCtrllerInstId |
Physical Instance ID of EDMA3 Controller
EDMA3_DRV_ObjState EDMA3_DRV_Object::state |
State information of the EDMA3 Driver object
uint32_t EDMA3_DRV_Object::numOpens |
Number of EDMA3 Driver instances
Init-time Configuration structure for EDMA3 controller, to provide Global SoC specific Information.
This configuration info can be provided by the user at run-time, while calling EDMA3_DRV_create(). If not provided at run-time, this info will be taken from the config file edma3Cfg.c.