Event queue priorities setup. More...
#include <edma3_drv.h>
Data Fields | |
uint32_t | evtQPri [EDMA3_MAX_EVT_QUE] |
Event Queue Priorities. |
Event queue priorities setup.
It allows to change the priority of the individual queues and the priority of the transfer request (TR) associated with the events queued in the queue.