EDMA3 Driver Enums
[EDMA3 Driver Symbols]

Enumerations

enum  EDMA3_DRV_HW_CHANNEL_EVENT {
  EDMA3_DRV_HW_CHANNEL_EVENT_0 = 0,
  EDMA3_DRV_HW_CHANNEL_EVENT_1,
  EDMA3_DRV_HW_CHANNEL_EVENT_2,
  EDMA3_DRV_HW_CHANNEL_EVENT_3,
  EDMA3_DRV_HW_CHANNEL_EVENT_4,
  EDMA3_DRV_HW_CHANNEL_EVENT_5,
  EDMA3_DRV_HW_CHANNEL_EVENT_6,
  EDMA3_DRV_HW_CHANNEL_EVENT_7,
  EDMA3_DRV_HW_CHANNEL_EVENT_8,
  EDMA3_DRV_HW_CHANNEL_EVENT_9,
  EDMA3_DRV_HW_CHANNEL_EVENT_10,
  EDMA3_DRV_HW_CHANNEL_EVENT_11,
  EDMA3_DRV_HW_CHANNEL_EVENT_12,
  EDMA3_DRV_HW_CHANNEL_EVENT_13,
  EDMA3_DRV_HW_CHANNEL_EVENT_14,
  EDMA3_DRV_HW_CHANNEL_EVENT_15,
  EDMA3_DRV_HW_CHANNEL_EVENT_16,
  EDMA3_DRV_HW_CHANNEL_EVENT_17,
  EDMA3_DRV_HW_CHANNEL_EVENT_18,
  EDMA3_DRV_HW_CHANNEL_EVENT_19,
  EDMA3_DRV_HW_CHANNEL_EVENT_20,
  EDMA3_DRV_HW_CHANNEL_EVENT_21,
  EDMA3_DRV_HW_CHANNEL_EVENT_22,
  EDMA3_DRV_HW_CHANNEL_EVENT_23,
  EDMA3_DRV_HW_CHANNEL_EVENT_24,
  EDMA3_DRV_HW_CHANNEL_EVENT_25,
  EDMA3_DRV_HW_CHANNEL_EVENT_26,
  EDMA3_DRV_HW_CHANNEL_EVENT_27,
  EDMA3_DRV_HW_CHANNEL_EVENT_28,
  EDMA3_DRV_HW_CHANNEL_EVENT_29,
  EDMA3_DRV_HW_CHANNEL_EVENT_30,
  EDMA3_DRV_HW_CHANNEL_EVENT_31,
  EDMA3_DRV_HW_CHANNEL_EVENT_32,
  EDMA3_DRV_HW_CHANNEL_EVENT_33,
  EDMA3_DRV_HW_CHANNEL_EVENT_34,
  EDMA3_DRV_HW_CHANNEL_EVENT_35,
  EDMA3_DRV_HW_CHANNEL_EVENT_36,
  EDMA3_DRV_HW_CHANNEL_EVENT_37,
  EDMA3_DRV_HW_CHANNEL_EVENT_38,
  EDMA3_DRV_HW_CHANNEL_EVENT_39,
  EDMA3_DRV_HW_CHANNEL_EVENT_40,
  EDMA3_DRV_HW_CHANNEL_EVENT_41,
  EDMA3_DRV_HW_CHANNEL_EVENT_42,
  EDMA3_DRV_HW_CHANNEL_EVENT_43,
  EDMA3_DRV_HW_CHANNEL_EVENT_44,
  EDMA3_DRV_HW_CHANNEL_EVENT_45,
  EDMA3_DRV_HW_CHANNEL_EVENT_46,
  EDMA3_DRV_HW_CHANNEL_EVENT_47,
  EDMA3_DRV_HW_CHANNEL_EVENT_48,
  EDMA3_DRV_HW_CHANNEL_EVENT_49,
  EDMA3_DRV_HW_CHANNEL_EVENT_50,
  EDMA3_DRV_HW_CHANNEL_EVENT_51,
  EDMA3_DRV_HW_CHANNEL_EVENT_52,
  EDMA3_DRV_HW_CHANNEL_EVENT_53,
  EDMA3_DRV_HW_CHANNEL_EVENT_54,
  EDMA3_DRV_HW_CHANNEL_EVENT_55,
  EDMA3_DRV_HW_CHANNEL_EVENT_56,
  EDMA3_DRV_HW_CHANNEL_EVENT_57,
  EDMA3_DRV_HW_CHANNEL_EVENT_58,
  EDMA3_DRV_HW_CHANNEL_EVENT_59,
  EDMA3_DRV_HW_CHANNEL_EVENT_60,
  EDMA3_DRV_HW_CHANNEL_EVENT_61,
  EDMA3_DRV_HW_CHANNEL_EVENT_62,
  EDMA3_DRV_HW_CHANNEL_EVENT_63
}
 

DMA Channels assigned to different Hardware Events.

More...
enum  EDMA3_DRV_OptField {
  EDMA3_DRV_OPT_FIELD_SAM = 0,
  EDMA3_DRV_OPT_FIELD_DAM = 1,
  EDMA3_DRV_OPT_FIELD_SYNCDIM = 2,
  EDMA3_DRV_OPT_FIELD_STATIC = 3,
  EDMA3_DRV_OPT_FIELD_FWID = 4,
  EDMA3_DRV_OPT_FIELD_TCCMODE = 5,
  EDMA3_DRV_OPT_FIELD_TCC = 6,
  EDMA3_DRV_OPT_FIELD_TCINTEN = 7,
  EDMA3_DRV_OPT_FIELD_ITCINTEN = 8,
  EDMA3_DRV_OPT_FIELD_TCCHEN = 9,
  EDMA3_DRV_OPT_FIELD_ITCCHEN = 10
}
 

OPT Field Offset.

More...
enum  EDMA3_DRV_AddrMode {
  EDMA3_DRV_ADDR_MODE_INCR = 0,
  EDMA3_DRV_ADDR_MODE_FIFO = 1
}
 

EDMA Addressing modes.

More...
enum  EDMA3_DRV_SyncType {
  EDMA3_DRV_SYNC_A = 0,
  EDMA3_DRV_SYNC_AB = 1
}
 

EDMA Transfer Synchronization type.

More...
enum  EDMA3_DRV_StaticMode {
  EDMA3_DRV_STATIC_DIS = 0,
  EDMA3_DRV_STATIC_EN = 1
}
 

True/False: PaRAM set is Static or not. A Static PaRAM set is updated or linked after TR is submitted.

More...
enum  EDMA3_DRV_FifoWidth {
  EDMA3_DRV_W8BIT = 0,
  EDMA3_DRV_W16BIT = 1,
  EDMA3_DRV_W32BIT = 2,
  EDMA3_DRV_W64BIT = 3,
  EDMA3_DRV_W128BIT = 4,
  EDMA3_DRV_W256BIT = 5
}
 

EDMA3 FIFO width.

More...
enum  EDMA3_DRV_TccMode {
  EDMA3_DRV_TCCMODE_NORMAL = 0,
  EDMA3_DRV_TCCMODE_EARLY = 1
}
 

Transfer complete code mode. Indicates the point at which a transfer is considered completed for chaining and interrupt generation.

More...
enum  EDMA3_DRV_TcintEn {
  EDMA3_DRV_TCINTEN_DIS = 0,
  EDMA3_DRV_TCINTEN_EN = 1
}
 

Transfer complete interrupt enable.

More...
enum  EDMA3_DRV_ItcintEn {
  EDMA3_DRV_ITCINTEN_DIS = 0,
  EDMA3_DRV_ITCINTEN_EN = 1
}
 

Intermediate Transfer complete interrupt enable.

More...
enum  EDMA3_DRV_TcchEn {
  EDMA3_DRV_TCCHEN_DIS = 0,
  EDMA3_DRV_TCCHEN_EN = 1
}
 

Transfer complete chaining enable.

More...
enum  EDMA3_DRV_ItcchEn {
  EDMA3_DRV_ITCCHEN_DIS = 0,
  EDMA3_DRV_ITCCHEN_EN = 1
}
 

Intermediate Transfer complete chaining enable.

More...
enum  EDMA3_DRV_TrigMode {
  EDMA3_DRV_TRIG_MODE_MANUAL = 0,
  EDMA3_DRV_TRIG_MODE_QDMA = 1,
  EDMA3_DRV_TRIG_MODE_EVENT = 2,
  EDMA3_DRV_TRIG_MODE_NONE = 3
}
 

EDMA Trigger Mode Selection.

More...
enum  EDMA3_DRV_PaRAMEntry {
  EDMA3_DRV_PARAM_ENTRY_OPT = 0,
  EDMA3_DRV_PARAM_ENTRY_SRC = 1,
  EDMA3_DRV_PARAM_ENTRY_ACNT_BCNT = 2,
  EDMA3_DRV_PARAM_ENTRY_DST = 3,
  EDMA3_DRV_PARAM_ENTRY_SRC_DST_BIDX = 4,
  EDMA3_DRV_PARAM_ENTRY_LINK_BCNTRLD = 5,
  EDMA3_DRV_PARAM_ENTRY_SRC_DST_CIDX = 6,
  EDMA3_DRV_PARAM_ENTRY_CCNT = 7
}
 

PaRAM Set Entry type.

More...
enum  EDMA3_DRV_PaRAMField {
  EDMA3_DRV_PARAM_FIELD_OPT = 0,
  EDMA3_DRV_PARAM_FIELD_SRCADDR = 1,
  EDMA3_DRV_PARAM_FIELD_ACNT = 2,
  EDMA3_DRV_PARAM_FIELD_BCNT = 3,
  EDMA3_DRV_PARAM_FIELD_DESTADDR = 4,
  EDMA3_DRV_PARAM_FIELD_SRCBIDX = 5,
  EDMA3_DRV_PARAM_FIELD_DESTBIDX = 6,
  EDMA3_DRV_PARAM_FIELD_LINKADDR = 7,
  EDMA3_DRV_PARAM_FIELD_BCNTRELOAD = 8,
  EDMA3_DRV_PARAM_FIELD_SRCCIDX = 9,
  EDMA3_DRV_PARAM_FIELD_DESTCIDX = 10,
  EDMA3_DRV_PARAM_FIELD_CCNT = 11
}
 

PaRAM Set Field type.

More...
enum  EDMA3_DRV_IoctlCmd { ,
  EDMA3_DRV_IOCTL_SET_PARAM_CLEAR_OPTION,
  EDMA3_DRV_IOCTL_GET_PARAM_CLEAR_OPTION
}
 

EDMA3 Driver IOCTL commands.

More...
enum  EDMA3_DRV_Tc_Err {
  EDMA3_DRV_TC_ERR_BUSERR_DIS = 0,
  EDMA3_DRV_TC_ERR_BUSERR_EN,
  EDMA3_DRV_TC_ERR_TRERR_DIS,
  EDMA3_DRV_TC_ERR_TRERR_EN,
  EDMA3_DRV_TC_ERR_MMRAERR_DIS,
  EDMA3_DRV_TC_ERR_MMRAERR_EN,
  EDMA3_DRV_TC_ERR_DIS,
  EDMA3_DRV_TC_ERR_EN
}
 

TC Error Enablers.

More...

Enumeration Type Documentation

DMA Channels assigned to different Hardware Events.

They should be used while requesting a specific DMA channel. One possible usage is to maintain a SoC specific file, which will contain the mapping of these hardware events to the respective peripherals for better understanding and lesser probability of errors. Also, if any event associated with a particular peripheral gets changed, only that SoC specific file needs to be changed. for eg, the sample SoC specific file "soc.h" can have these defines:

define EDMA3_DRV_HW_CHANNEL_MCBSP_TX EDMA3_DRV_HW_CHANNEL_EVENT_2 define EDMA3_DRV_HW_CHANNEL_MCBSP_RX EDMA3_DRV_HW_CHANNEL_EVENT_3

These defines will be used by the MCBSP driver. The same event EDMA3_DRV_HW_CHANNEL_EVENT_2/3 could be mapped to some other peripheral also.

Enumerator:
EDMA3_DRV_HW_CHANNEL_EVENT_0 

Channel assigned to EDMA3 Event 0

EDMA3_DRV_HW_CHANNEL_EVENT_1 

Channel assigned to EDMA3 Event 1

EDMA3_DRV_HW_CHANNEL_EVENT_2 

Channel assigned to EDMA3 Event 2

EDMA3_DRV_HW_CHANNEL_EVENT_3 

Channel assigned to EDMA3 Event 3

EDMA3_DRV_HW_CHANNEL_EVENT_4 

Channel assigned to EDMA3 Event 4

EDMA3_DRV_HW_CHANNEL_EVENT_5 

Channel assigned to EDMA3 Event 5

EDMA3_DRV_HW_CHANNEL_EVENT_6 

Channel assigned to EDMA3 Event 6

EDMA3_DRV_HW_CHANNEL_EVENT_7 

Channel assigned to EDMA3 Event 7

EDMA3_DRV_HW_CHANNEL_EVENT_8 

Channel assigned to EDMA3 Event 8

EDMA3_DRV_HW_CHANNEL_EVENT_9 

Channel assigned to EDMA3 Event 9

EDMA3_DRV_HW_CHANNEL_EVENT_10 

Channel assigned to EDMA3 Event 10

EDMA3_DRV_HW_CHANNEL_EVENT_11 

Channel assigned to EDMA3 Event 11

EDMA3_DRV_HW_CHANNEL_EVENT_12 

Channel assigned to EDMA3 Event 12

EDMA3_DRV_HW_CHANNEL_EVENT_13 

Channel assigned to EDMA3 Event 13

EDMA3_DRV_HW_CHANNEL_EVENT_14 

Channel assigned to EDMA3 Event 14

EDMA3_DRV_HW_CHANNEL_EVENT_15 

Channel assigned to EDMA3 Event 15

EDMA3_DRV_HW_CHANNEL_EVENT_16 

Channel assigned to EDMA3 Event 16

EDMA3_DRV_HW_CHANNEL_EVENT_17 

Channel assigned to EDMA3 Event 17

EDMA3_DRV_HW_CHANNEL_EVENT_18 

Channel assigned to EDMA3 Event 18

EDMA3_DRV_HW_CHANNEL_EVENT_19 

Channel assigned to EDMA3 Event 19

EDMA3_DRV_HW_CHANNEL_EVENT_20 

Channel assigned to EDMA3 Event 20

EDMA3_DRV_HW_CHANNEL_EVENT_21 

Channel assigned to EDMA3 Event 21

EDMA3_DRV_HW_CHANNEL_EVENT_22 

Channel assigned to EDMA3 Event 22

EDMA3_DRV_HW_CHANNEL_EVENT_23 

Channel assigned to EDMA3 Event 23

EDMA3_DRV_HW_CHANNEL_EVENT_24 

Channel assigned to EDMA3 Event 24

EDMA3_DRV_HW_CHANNEL_EVENT_25 

Channel assigned to EDMA3 Event 25

EDMA3_DRV_HW_CHANNEL_EVENT_26 

Channel assigned to EDMA3 Event 26

EDMA3_DRV_HW_CHANNEL_EVENT_27 

Channel assigned to EDMA3 Event 27

EDMA3_DRV_HW_CHANNEL_EVENT_28 

Channel assigned to EDMA3 Event 28

EDMA3_DRV_HW_CHANNEL_EVENT_29 

Channel assigned to EDMA3 Event 29

EDMA3_DRV_HW_CHANNEL_EVENT_30 

Channel assigned to EDMA3 Event 30

EDMA3_DRV_HW_CHANNEL_EVENT_31 

Channel assigned to EDMA3 Event 31

EDMA3_DRV_HW_CHANNEL_EVENT_32 

Channel assigned to EDMA3 Event 32

EDMA3_DRV_HW_CHANNEL_EVENT_33 

Channel assigned to EDMA3 Event 33

EDMA3_DRV_HW_CHANNEL_EVENT_34 

Channel assigned to EDMA3 Event 34

EDMA3_DRV_HW_CHANNEL_EVENT_35 

Channel assigned to EDMA3 Event 35

EDMA3_DRV_HW_CHANNEL_EVENT_36 

Channel assigned to EDMA3 Event 36

EDMA3_DRV_HW_CHANNEL_EVENT_37 

Channel assigned to EDMA3 Event 37

EDMA3_DRV_HW_CHANNEL_EVENT_38 

Channel assigned to EDMA3 Event 38

EDMA3_DRV_HW_CHANNEL_EVENT_39 

Channel assigned to EDMA3 Event 39

EDMA3_DRV_HW_CHANNEL_EVENT_40 

Channel assigned to EDMA3 Event 40

EDMA3_DRV_HW_CHANNEL_EVENT_41 

Channel assigned to EDMA3 Event 41

EDMA3_DRV_HW_CHANNEL_EVENT_42 

Channel assigned to EDMA3 Event 42

EDMA3_DRV_HW_CHANNEL_EVENT_43 

Channel assigned to EDMA3 Event 43

EDMA3_DRV_HW_CHANNEL_EVENT_44 

Channel assigned to EDMA3 Event 44

EDMA3_DRV_HW_CHANNEL_EVENT_45 

Channel assigned to EDMA3 Event 45

EDMA3_DRV_HW_CHANNEL_EVENT_46 

Channel assigned to EDMA3 Event 46

EDMA3_DRV_HW_CHANNEL_EVENT_47 

Channel assigned to EDMA3 Event 47

EDMA3_DRV_HW_CHANNEL_EVENT_48 

Channel assigned to EDMA3 Event 48

EDMA3_DRV_HW_CHANNEL_EVENT_49 

Channel assigned to EDMA3 Event 49

EDMA3_DRV_HW_CHANNEL_EVENT_50 

Channel assigned to EDMA3 Event 50

EDMA3_DRV_HW_CHANNEL_EVENT_51 

Channel assigned to EDMA3 Event 51

EDMA3_DRV_HW_CHANNEL_EVENT_52 

Channel assigned to EDMA3 Event 52

EDMA3_DRV_HW_CHANNEL_EVENT_53 

Channel assigned to EDMA3 Event 53

EDMA3_DRV_HW_CHANNEL_EVENT_54 

Channel assigned to EDMA3 Event 54

EDMA3_DRV_HW_CHANNEL_EVENT_55 

Channel assigned to EDMA3 Event 55

EDMA3_DRV_HW_CHANNEL_EVENT_56 

Channel assigned to EDMA3 Event 56

EDMA3_DRV_HW_CHANNEL_EVENT_57 

Channel assigned to EDMA3 Event 57

EDMA3_DRV_HW_CHANNEL_EVENT_58 

Channel assigned to EDMA3 Event 58

EDMA3_DRV_HW_CHANNEL_EVENT_59 

Channel assigned to EDMA3 Event 59

EDMA3_DRV_HW_CHANNEL_EVENT_60 

Channel assigned to EDMA3 Event 60

EDMA3_DRV_HW_CHANNEL_EVENT_61 

Channel assigned to EDMA3 Event 61

EDMA3_DRV_HW_CHANNEL_EVENT_62 

Channel assigned to EDMA3 Event 62

EDMA3_DRV_HW_CHANNEL_EVENT_63 

Channel assigned to EDMA3 Event 63

OPT Field Offset.

Use this enum to set or get any of the Fields within an OPT of a Parameter RAM set.

Enumerator:
EDMA3_DRV_OPT_FIELD_SAM 

Source addressing mode (INCR / FIFO) (Bit 0)

EDMA3_DRV_OPT_FIELD_DAM 

Destination addressing mode (INCR / FIFO) (Bit 1)

EDMA3_DRV_OPT_FIELD_SYNCDIM 

Transfer synchronization dimension (A-synchronized / AB-synchronized) (Bit 2)

EDMA3_DRV_OPT_FIELD_STATIC 

The STATIC field PaRAM set is static/non-static? (Bit 3)

EDMA3_DRV_OPT_FIELD_FWID 

FIFO Width. Applies if either SAM or DAM is set to FIFO mode. (Bitfield 8-10)

EDMA3_DRV_OPT_FIELD_TCCMODE 

Transfer complete code mode. Indicates the point at which a transfer is considered completed for chaining and interrupt generation. (Bit 11)

EDMA3_DRV_OPT_FIELD_TCC 

Transfer Complete Code (TCC). This 6-bit code is used to set the relevant bit in chaining enable register (CER[TCC]/CERH[TCC]) for chaining or in interrupt pending register (IPR[TCC]/IPRH[TCC]) for interrupts. (Bitfield 12-17)

EDMA3_DRV_OPT_FIELD_TCINTEN 

Transfer complete interrupt enable/disable. (Bit 20)

EDMA3_DRV_OPT_FIELD_ITCINTEN 

Intermediate transfer complete interrupt enable/disable. (Bit 21)

EDMA3_DRV_OPT_FIELD_TCCHEN 

Transfer complete chaining enable/disable (Bit 22)

EDMA3_DRV_OPT_FIELD_ITCCHEN 

Intermediate transfer completion chaining enable/disable (Bit 23)

EDMA Addressing modes.

The EDMA3 TC supports two addressing modes

  1. Increment transfer
  2. FIFO transfer

The SAM (Source Addressing Mode) and the DAM (Destination Addressing Mode) can be independently set to either of the two via the OPT register.

Enumerator:
EDMA3_DRV_ADDR_MODE_INCR 

Increment (INCR) mode. Source addressing within an array increments. Source is not a FIFO.

EDMA3_DRV_ADDR_MODE_FIFO 

FIFO mode. Source addressing within an array wraps around upon reaching FIFO width.

EDMA Transfer Synchronization type.

Two types of Synchronization of transfers are possible

  1. A Synchronized
  2. AB Syncronized

A Sync

  1. Each Array is submitted as one TR
  2. (BCNT*CCNT) number of sync events are needed to completely service a PaRAM set. (Where BCNT = Num of Arrays in a Frame; CCNT = Num of Frames in a Block)
  3. (S/D)CIDX = (Addr of First array in next frame) minus (Addr of Last array in present frame) (Where CIDX is the Inter-Frame index)
  • AB Sync
    1. Each Frame is submitted as one TR
    2. Only CCNT number of sync events are needed to completely service a PaRAM set
    3. (S/D)CIDX = (Addr of First array in next frame) minus (Addr of First array of present frame)
Note:
ABC sync transfers can be achieved logically by chaining multiple AB sync transfers
Enumerator:
EDMA3_DRV_SYNC_A 

A-synchronized. Each event triggers the transfer of a single array of ACNT bytes

EDMA3_DRV_SYNC_AB 

AB-synchronized. Each event triggers the transfer of BCNT arrays of ACNT bytes

True/False: PaRAM set is Static or not. A Static PaRAM set is updated or linked after TR is submitted.

Enumerator:
EDMA3_DRV_STATIC_DIS 

PaRAM set is not Static. PaRAM set is updated or linked after TR is submitted. A value of 0 should be used for DMA channels and for nonfinal transfers in a linked list of QDMA transfers

EDMA3_DRV_STATIC_EN 

PaRAM set is Static. PaRAM set is not updated or linked after TR is submitted. A value of 1 should be used for isolated QDMA transfers or for the final transfer in a linked list of QDMA transfers.

EDMA3 FIFO width.

The user can set the width of the FIFO using this enum. This is done via the OPT register. This is valid only if the EDMA3_DRV_ADDR_MODE_FIFO value is used for the enum EDMA3_DRV_AddrMode.

Enumerator:
EDMA3_DRV_W8BIT 

FIFO width is 8-bit.

EDMA3_DRV_W16BIT 

FIFO width is 16-bit.

EDMA3_DRV_W32BIT 

FIFO width is 32-bit.

EDMA3_DRV_W64BIT 

FIFO width is 64-bit.

EDMA3_DRV_W128BIT 

FIFO width is 128-bit.

EDMA3_DRV_W256BIT 

FIFO width is 256-bit.

Transfer complete code mode. Indicates the point at which a transfer is considered completed for chaining and interrupt generation.

Enumerator:
EDMA3_DRV_TCCMODE_NORMAL 

A transfer is considered completed after transfer of data

EDMA3_DRV_TCCMODE_EARLY 

A transfer is considered completed after the EDMA3CC submits a TR to the EDMA3TC. TC may still be transferring data when interrupt/chain is triggered.

Transfer complete interrupt enable.

Enumerator:
EDMA3_DRV_TCINTEN_DIS 

Transfer complete interrupt is disabled

EDMA3_DRV_TCINTEN_EN 

Transfer complete interrupt is enabled. When enabled, the interrupt pending register (IPR/IPRH) bit is set on transfer completion (upon completion of the final TR in the PaRAM set). The bit (position) set in IPR or IPRH is the TCC value specified. In order to generate a completion interrupt to the CPU, the corresponding IER [TCC] / IERH [TCC] bit must be set to 1.

Intermediate Transfer complete interrupt enable.

Enumerator:
EDMA3_DRV_ITCINTEN_DIS 

Intermediate Transfer complete interrupt is disabled

EDMA3_DRV_ITCINTEN_EN 

Intermediate transfer complete interrupt is enabled. When enabled, the interrupt pending register (IPR/IPRH) bit is set on every intermediate transfer completion (upon completion of every intermediate TR in the PaRAM set, except the final TR in the PaRAM set). The bit (position) set in IPR or IPRH is the TCC value specified. In order to generate a completion interrupt to the CPU, the corresponding IER [TCC] / IERH [TCC] bit must be set to 1.

Transfer complete chaining enable.

Enumerator:
EDMA3_DRV_TCCHEN_DIS 

Transfer complete chaining is disabled

EDMA3_DRV_TCCHEN_EN 

Transfer complete chaining is enabled. When enabled, the chained event register (CER/CERH) bit is set on final chained transfer completion (upon completion of the final / last TR in the PaRAM set). The bit (position) set in CER or CERH is the TCC value specified.

Intermediate Transfer complete chaining enable.

Enumerator:
EDMA3_DRV_ITCCHEN_DIS 

Intermediate Transfer complete chaining is disabled

EDMA3_DRV_ITCCHEN_EN 

Intermediate transfer complete chaining is enabled. When enabled, the chained event register (CER/CERH) bit is set on every intermediate chained transfer completion (upon completion of every intermediate TR in the PaRAM set, except the final TR in the PaRAM set). The bit (position) set in CER or CERH is the TCC value specified.

EDMA Trigger Mode Selection.

Use this enum to select the EDMA trigger mode while enabling the EDMA transfer

Enumerator:
EDMA3_DRV_TRIG_MODE_MANUAL 

Set the Trigger mode to Manual . The CPU manually triggers a transfer by writing a 1 to the corresponding bit in the event set register (ESR/ESRH).

EDMA3_DRV_TRIG_MODE_QDMA 

Set the Trigger mode to QDMA. A QDMA transfer is triggered when a CPU (or other EDMA3 programmer) writes to the trigger word of the QDMA channel parameter set (autotriggered) or when the EDMA3CC performs a link update on a PaRAM set that has been mapped to a QDMA channel (link triggered).

EDMA3_DRV_TRIG_MODE_EVENT 

Set the Trigger mode to Event. Allows for a peripheral, system, or externally-generated event to trigger a transfer request.

EDMA3_DRV_TRIG_MODE_NONE 

Used to specify the trigger mode NONE

PaRAM Set Entry type.

Use this enum to set or get any of the 8 DWords(unsigned int) within a Parameter RAM set

Enumerator:
EDMA3_DRV_PARAM_ENTRY_OPT 

The OPT field (Offset Address 0x0 Bytes)

EDMA3_DRV_PARAM_ENTRY_SRC 

The SRC field (Offset Address 0x4 Bytes)

EDMA3_DRV_PARAM_ENTRY_ACNT_BCNT 

The (ACNT+BCNT) field (Offset Address 0x8 Bytes)

EDMA3_DRV_PARAM_ENTRY_DST 

The DST field (Offset Address 0xC Bytes)

EDMA3_DRV_PARAM_ENTRY_SRC_DST_BIDX 

The (SRCBIDX+DSTBIDX) field (Offset Address 0x10 Bytes)

EDMA3_DRV_PARAM_ENTRY_LINK_BCNTRLD 

The (LINK+BCNTRLD) field (Offset Address 0x14 Bytes)

EDMA3_DRV_PARAM_ENTRY_SRC_DST_CIDX 

The (SRCCIDX+DSTCIDX) field (Offset Address 0x18 Bytes)

EDMA3_DRV_PARAM_ENTRY_CCNT 

The (CCNT+RSVD) field (Offset Address 0x1C Bytes)

PaRAM Set Field type.

Use this enum to set or get any of the PaRAM set fields

Enumerator:
EDMA3_DRV_PARAM_FIELD_OPT 

OPT field of PaRAM Set

EDMA3_DRV_PARAM_FIELD_SRCADDR 

Starting byte address of Source For FIFO mode, srcAddr must be a 256-bit aligned address.

EDMA3_DRV_PARAM_FIELD_ACNT 

Number of bytes in each Array (ACNT).

EDMA3_DRV_PARAM_FIELD_BCNT 

Number of Arrays in each Frame (BCNT).

EDMA3_DRV_PARAM_FIELD_DESTADDR 

Starting byte address of destination For FIFO mode, destAddr must be a 256-bit aligned address.

EDMA3_DRV_PARAM_FIELD_SRCBIDX 

Index between consec. arrays of a Source Frame (SRCBIDX) If SAM is set to 1 (via channelOptions) then srcInterArrIndex should be an even multiple of 32 bytes.

EDMA3_DRV_PARAM_FIELD_DESTBIDX 

Index between consec. arrays of a Destination Frame (DSTBIDX) If DAM is set to 1 (via channelOptions) then destInterArrIndex should be an even multiple of 32 bytes.

EDMA3_DRV_PARAM_FIELD_LINKADDR 

Address for linking (AutoReloading of a PaRAM Set) This must point to a valid aligned 32-byte PaRAM set A value of 0xFFFF means no linking Linking is especially useful for use with ping-pong buffers and circular buffers.

EDMA3_DRV_PARAM_FIELD_BCNTRELOAD 

Reload value of the numArrInFrame (BCNT) Relevant only for A-sync transfers.

EDMA3_DRV_PARAM_FIELD_SRCCIDX 

Index between consecutive frames of a Source Block (SRCCIDX).

EDMA3_DRV_PARAM_FIELD_DESTCIDX 

Index between consecutive frames of a Dest Block (DSTCIDX).

EDMA3_DRV_PARAM_FIELD_CCNT 

Number of Frames in a block (CCNT).

EDMA3 Driver IOCTL commands.

Enumerator:
EDMA3_DRV_IOCTL_SET_PARAM_CLEAR_OPTION 

PaRAM Sets will be cleared OR will not be cleared during allocation, depending upon this option.

For e.g., To clear the PaRAM Sets during allocation, cmdArg = (void *)1;

To NOT clear the PaRAM Sets during allocation, cmdArg = (void *)0;

For all other values, it will return error.

By default, PaRAM Sets will be cleared during allocation. Note: Since this enum can change the behavior how the resources are initialized during their allocation, user is adviced to not use this command while allocating the resources. User should first change the behavior of resources' initialization and then should use start allocating resources.

EDMA3_DRV_IOCTL_GET_PARAM_CLEAR_OPTION 

To check whether PaRAM Sets will be cleared or not during allocation. If the value read is '1', it means that PaRAM Sets are getting cleared during allocation. If the value read is '0', it means that PaRAM Sets are NOT getting cleared during allocation. For e.g., unsigned short isParamClearingDone; cmdArg =

TC Error Enablers.

Use this enum to enable/disable the specific EDMA3 Transfer Controller Interrupts.

Enumerator:
EDMA3_DRV_TC_ERR_BUSERR_DIS 

Interrupt disable for bus error

EDMA3_DRV_TC_ERR_BUSERR_EN 

Interrupt enable for bus error

EDMA3_DRV_TC_ERR_TRERR_DIS 

Interrupt disable for transfer request error

EDMA3_DRV_TC_ERR_TRERR_EN 

Interrupt enable for transfer request error

EDMA3_DRV_TC_ERR_MMRAERR_DIS 

Interrupt disable for MMR address error

EDMA3_DRV_TC_ERR_MMRAERR_EN 

Interrupt enable for MMR address error

EDMA3_DRV_TC_ERR_DIS 

Disable all TC error interrupts

EDMA3_DRV_TC_ERR_EN 

Enable all TC error interrupts


Generated on Fri Jan 28 15:45:38 2011 for EDMA3 Driver by  doxygen 1.6.1