XDAIS
dais-x04
|
Defines the creation time parameters for all IVIDANALYTICS instance objects. More...
#include <ividanalytics.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | maxHeight |
XDAS_Int32 | maxWidth |
XDAS_Int32 | maxFrameRate |
XDAS_Int32 | dataEndianness |
XDAS_Int32 | inputChromaFormat |
XDAS_Int32 | maxRules |
Defines the creation time parameters for all IVIDANALYTICS instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. XDAS_Int32 IVIDANALYTICS_Params::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDANALYTICS_Params::maxHeight |
Maximum video height in pixels.
XDAS_Int32 IVIDANALYTICS_Params::maxWidth |
Maximum video width in pixels.
XDAS_Int32 IVIDANALYTICS_Params::maxFrameRate |
Maximum frame rate in fps * 1000. For example, if max frame rate is 30 frames per second, set this field to 30000.
XDAS_Int32 IVIDANALYTICS_Params::dataEndianness |
Endianness of output data.
XDAS_Int32 IVIDANALYTICS_Params::inputChromaFormat |
Chroma format for the input buffer.
XDAS_Int32 IVIDANALYTICS_Params::maxRules |
Maximum number of rules allowed.