IAUDDEC1_Params Struct Reference
[XDM IAUDDEC1 Audio Decoder Interface]

Defines the creation time parameters for all IAUDDEC1 instance objects. More...

#include <iauddec1.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 outputPCMWidth
XDAS_Int32 pcmFormat
XDAS_Int32 dataEndianness

Detailed Description

Defines the creation time parameters for all IAUDDEC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller.

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Number of bits per output PCM Sample.

Output PCM Format Block/Interleaved.

See also:
IAUDIO_PcmFormat

Endianness of output data.

See also:
XDM_DataFormat

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated