The XDAIS interfaces are comprised of the following:
The XDM interfaces included in this release are comprised of the following:
These older XDM interfaces continue to be supported, but also continue to be deprecated in this release. These interfaces are comprised of the following:
And finally, there are a few beta interfaces provided with this release. They are available for review, and comments are welcome. Each beta interface will be reviewed and updated with customer feedback, and when appropriate, upgraded to a supported interface in a future release.