Defines the run time output arguments for all IVIDENC instance objects. More...
#include <ividenc.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
XDAS_Int32 | bytesGenerated |
XDAS_Int32 | encodedFrameType |
XDAS_Int32 | inputFrameSkip |
IVIDEO_BufDesc | reconBufs |
Defines the run time output arguments for all IVIDENC instance objects.
size
parameter. size
field must be correctly set by the caller.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Extended error information.
Bytes generated by the encode.
Video frame types.
IVIDEO_xy_FRAME
values, this frame type is interlaced where both top and bottom fields are provided in a single frame. The first field is an "x" frame, the second field is "y" field.Frame Skip Mode. See IVIDEO_SkipMode.
Reconstruction Frames.