IVIDDEC2_Fxns Struct Reference
[XDM IVIDDEC2 Video Decoder Interface]

Defines all of the operations on IVIDDEC2 objects. More...

#include <ividdec2.h>

Collaboration diagram for IVIDDEC2_Fxns:
Collaboration graph
[legend]

Data Fields

IALG_Fxns ialg
XDAS_Int32(* process )(IVIDDEC2_Handle handle, XDM1_BufDesc *inBufs, XDM_BufDesc *outBufs, IVIDDEC2_InArgs *inArgs, IVIDDEC2_OutArgs *outArgs)
 Basic video decoding call.
XDAS_Int32(* control )(IVIDDEC2_Handle handle, IVIDDEC2_Cmd id, IVIDDEC2_DynamicParams *params, IVIDDEC2_Status *status)
 Control behavior of an algorithm.

Detailed Description

Defines all of the operations on IVIDDEC2 objects.


Field Documentation

XDAIS algorithm interface.

See also:
IALG_Fxns

Basic video decoding call.

Parameters:
[in] handle Handle to an algorithm instance.
[in,out] inBufs Input buffer descriptors.
[in,out] outBufs Output buffer descriptors. The algorithm may modify the output buffer pointers.
[in] inArgs Input arguments. This is a required parameter.
[out] outArgs Ouput results. This is a required parameter.
Remarks:
process() is a blocking call. When process() returns, the algorithm's processing is complete.
process() enables codecs to support error resiliency and error concealment. As a result, even if IVIDDEC2_EFAIL is returned from process() because the encoded buffer has an error, it's possible that decoded buffers (outArgs->decodedBufs) and display buffers (outArgs->displayBufs) could still be returned. The codec can indicate that buffers are available by not setting the XDM_ISFATALERROR bit in the respective displayBufs and decodedBufs extendedError field if the buffers contain valid data.
By extension then, if the outArgs->decodedBufs and outArgs->displayBufs buffers are not valid, even if the codec's process() call returns IVIDDEC2_EFAIL, it must also be sure to set the XDM_ISFATALERROR bit in the respective extendedError fields. Failure to do so may result in applications accessing these buffers and causing system instability.
Precondition:
inBufs->numBufs will indicate the total number of input buffers supplied for input frame, and conditionally, the encoders MB data buffer.
If IVIDDEC2_DynamicParams::mbDataFlag was set to XDAS_FALSE in a previous control() call, the application only needs to provide buffers for reconstruction frames.
If IVIDDEC2_DynamicParams::mbDataFlag was set to XDAS_TRUE in a previous control() call, outBufs->bufs[outBufs->numBufs - 1] is a buffer descriptor into which the algorithm will write MB data for each macro block. The size of the MB data buffer will vary based on the decoder type. H.264 may generate N264 bytes per MB, while Mpeg2 may generate NMP2 bytes. The exact size of the buffers should be obtained by calling the algorithm's control() method with XDM_GETBUFINFO.
inArgs must not be NULL, and must point to a valid IVIDDEC2_InArgs structure.
outArgs must not be NULL, and must point to a valid IVIDDEC2_OutArgs structure.
inBufs must not be NULL, and must point to a valid XDM1_BufDesc structure.
inBufs->descs[0].buf must not be NULL, and must point to a valid buffer of data that is at least inBufs->descs[0].bufSize bytes in length.
outBufs must not be NULL, and must point to a valid XDM_BufDesc structure.
outBufs->buf[0] must not be NULL, and must point to a valid buffer of data that is at least outBufs->bufSizes[0] bytes in length.
The buffers in inBufs and outBufs are physically contiguous and owned by the calling application.
Postcondition:
The algorithm must not modify the contents of inArgs.
The algorithm must not modify the contents of inBufs, with the exception of inBufs.bufDesc[].accessMask. That is, the data and buffers pointed to by these parameters must be treated as read-only.
The algorithm must modify the contents of inBufs->descs[].accessMask and appropriately indicate the mode in which each of the buffers in inBufs were read. For example, if the algorithm only read from inBufs.descs[0].buf using the algorithm processor, it could utilize XDM_SETACCESSMODE_READ to update the appropriate accessMask fields. The application may utilize these returned values to appropriately manage cache.
The buffers in inBufs are owned by the calling application.
Return values:
IVIDDEC2_EOK Success.
IVIDDEC2_EFAIL General failure. See IVIDDEC2_Status::extendedError for more detailed further error conditions.
IVIDDEC2_EUNSUPPORTED Request is unsupported.

Control behavior of an algorithm.

Parameters:
[in] handle Handle to an algorithm instance.
[in] id Command id. See XDM_CmdId.
[in] params Dynamic parameters. This is a required parameter.
[out] status Output results. This is a required parameter.
Precondition:
handle must be a valid algorithm instance handle.
params must not be NULL, and must point to a valid IVIDDEC2_DynamicParams structure.
status must not be NULL, and must point to a valid IVIDDEC2_Status structure.
If a buffer is provided in the status->data field, it must be physically contiguous and owned by the calling application.
Postcondition:
The algorithm must not modify the contents of params. That is, the data pointed to by this parameter must be treated as read-only.
If a buffer was provided in the status->data field, it is owned by the calling application.
Return values:
IVIDDEC2_EOK Success.
IVIDDEC2_EFAIL General failure. See IVIDDEC2_Status::extendedError for more detailed further error conditions.
IVIDDEC2_EUNSUPPORTED Request is unsupported.

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated