Defines instance status parameters (read-only). More...
#include <iauddec.h>
Defines instance status parameters (read-only).
size
parameter. size
field must be correctly set by the caller.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Extended error information.
Average bit rate, in bits per second.
Sampling frequency, in Hz. For example, if the sampling frequency is 44.1 kHz, this field will be 44100.
Number of Channels. See IAUDIO_ChannelId.
Number of LFE (Low Frequency Effects) channels in the stream.
The output PCM format. See IAUDIO_PcmFormat.
Flag to indicate support for random position decoding, which means that a stream can be decoded from any point. 0 indicates this feature is not supported, 1 indicates this feature is supported.
Recommended fast forward length in bytes in case of random position decoding.
Number of samples decoded per process() call.
Number of bits per output sample. For example, if the value of the field is 16, there are 16 output bits per PCM sample.
Input and output buffer information. See XDM_AlgBufInfo.