XDM Audio Interface

Enumerations

enum  IAUDIO_ChannelId {
  IAUDIO_MONO = 0,
  IAUDIO_STEREO = 1,
  IAUDIO_THREE_ZERO = 2,
  IAUDIO_FIVE_ZERO = 3,
  IAUDIO_FIVE_ONE = 4,
  IAUDIO_SEVEN_ONE = 5
}
 

XDM supported audio channel configurations.

More...
enum  IAUDIO_ChannelMode {
  IAUDIO_1_0 = 0,
  IAUDIO_2_0 = 1,
  IAUDIO_11_0 = 2,
  IAUDIO_3_0 = 3,
  IAUDIO_2_1 = 4,
  IAUDIO_3_1 = 5,
  IAUDIO_2_2 = 6,
  IAUDIO_3_2 = 7,
  IAUDIO_2_3 = 8,
  IAUDIO_3_3 = 9,
  IAUDIO_3_4 = 10
}
 

Channel modes for audio streams.

More...
enum  IAUDIO_DualMonoMode {
  IAUDIO_DUALMONO_LR = 0,
  IAUDIO_DUALMONO_LEFT = 1,
  IAUDIO_DUALMONO_RIGHT = 2,
  IAUDIO_DUALMONO_LR_MIX = 3
}
 

Dual Mono Channel modes for audio streams.

More...
enum  IAUDIO_PcmFormat {
  IAUDIO_BLOCK = 0,
  IAUDIO_INTERLEAVED = 1
}
 

XDM supported audio PCM formats.

More...
enum  IAUDIO_EncMode {
  IAUDIO_CBR = 0,
  IAUDIO_VBR = 1
}
 

Audio encoding modes.

More...

Detailed Description

This is the XDM audio interface shared between the various codecs.


Enumeration Type Documentation

XDM supported audio channel configurations.

Deprecated:
This enumeration is only supported on 0.9 XDM. To use it, you must define "XDM_INCLUDE_DOT9_SUPPORT" prior to including this file. In XDM 1.00, this has been superceded by IAUDIO_ChannelMode.
Enumerator:
IAUDIO_MONO 

Single channel.

IAUDIO_STEREO 

Two channel.

IAUDIO_THREE_ZERO 

Three channel.

IAUDIO_FIVE_ZERO 

Five channel.

IAUDIO_FIVE_ONE 

5.1 channel.

IAUDIO_SEVEN_ONE 

7.1 channel.

Channel modes for audio streams.

The channel modes not only indicate the number of channels, but also indicate the order in which the channels are placed in the input or output buffer. The placement of channels is indicated next to each channel mode.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
Enumerator:
IAUDIO_1_0 

Mono.

IAUDIO_2_0 

Stereo.

IAUDIO_11_0 

Dual Mono.

See also:
IAUDIO_DualMonoMode
IAUDIO_3_0 

Left, Right, Center.

IAUDIO_2_1 

Left, Right, Sur.

IAUDIO_3_1 

Left, Right, Center, Sur.

IAUDIO_2_2 

Left, Right, SurL, SurR.

IAUDIO_3_2 

Left, Right, Center, SurL, SurR.

IAUDIO_2_3 

Left, Right, SurL, SurR, surC.

IAUDIO_3_3 

Left, Right, Center, SurL, SurR, surC.

IAUDIO_3_4 

Left, Right, Center, SurL, SurR, sideL, sideR.

Dual Mono Channel modes for audio streams.

Remarks:
In case of Dual Mono the application can play both channels; Left Only, Right Only or Mix and Play both. The default case in most of the applications is the first case of IAUDIO_DUALMONO_LR. That is to play both Left and Right Channel.
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
Enumerator:
IAUDIO_DUALMONO_LR 

Play/encode both left and right channel

IAUDIO_DUALMONO_LEFT 

Play/encode only left channel.

IAUDIO_DUALMONO_RIGHT 

Play/encode only right channel.

IAUDIO_DUALMONO_LR_MIX 

Mix and play.

XDM supported audio PCM formats.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
Enumerator:
IAUDIO_BLOCK 

Left channel data followed by right channel data. Note, for single channel (mono), right channel data will be the same as the left channel data.

IAUDIO_INTERLEAVED 

Left and right channel data interleaved. Note, for single channel (mono), right channel data will be the same as the left channel data.

Audio encoding modes.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
Enumerator:
IAUDIO_CBR 

Constant bit rate.

IAUDIO_VBR 

Variable bit rate.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated