Defines instance status parameters (read-only). More...
#include <iauddec1.h>
Defines instance status parameters (read-only).
size
parameter. size
field must be correctly set by the caller.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Extended error information.
Buffer descriptor for data passing.
Reflects the validity of this status structure.
Flag indicating the presence of LFE channel in the output. When the LFE channel is not in the output, this is set to XDAS_FALSE.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
Average bit rate, in bits per second.
Sampling frequency, in Hz. For example, if the sampling frequency is 44.1 kHz, this field will be 44100.
Output Channel Configuration.
Output PCM Format Block/Interleaved.
Number of samples in the output.
Number of bits per output sample. For example, if the value of the field is 16, there are 16 output bits per PCM sample.
Input and output buffer information.
Mode to indicate type of Dual Mono. Only used in case of Dual Mono Output.