iimgenc1.h File Reference


Detailed Description

This header defines all types, constants, and functions shared by all implementations of the image encoder algorithms.

#include <ti/xdais/ialg.h>
#include <ti/xdais/xdas.h>
#include "xdm.h"
Include dependency graph for iimgenc1.h:

Go to the source code of this file.

Data Structures

struct  IIMGENC1_Obj
 This must be the first field of all IIMGENC1 instance objects. More...
struct  IIMGENC1_Params
 Defines the creation time parameters for all IIMGENC1 instance objects. More...
struct  IIMGENC1_DynamicParams
 This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
struct  IIMGENC1_InArgs
 Defines the input arguments for all IIMGENC1 instance process() function. More...
struct  IIMGENC1_Status
 Defines instance status parameters. More...
struct  IIMGENC1_OutArgs
 Defines the run time output arguments for all IIMGENC1 instance objects. More...
struct  IIMGENC1_Fxns
 Defines all of the operations on IIMGENC1 objects. More...

Defines

#define IIMGENC1_EOK   XDM_EOK
#define IIMGENC1_EFAIL   XDM_EFAIL
#define IIMGENC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Typedefs

typedef struct IIMGENC1_ObjIIMGENC1_Handle
 Opaque handle to an IIMGENC1 objects.
typedef IALG_Cmd IIMGENC1_Cmd
 Defines the control commands for the IIMGENC1 module.
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated