This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
#include <iimgenc1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | numAU |
XDAS_Int32 | inputChromaFormat |
XDAS_Int32 | inputHeight |
XDAS_Int32 | inputWidth |
XDAS_Int32 | captureWidth |
XDAS_Int32 | generateHeader |
XDAS_Int32 | qValue |
This structure defines the algorithm parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Number of Access unit to encode. Set to XDM_DEFAULT to encode the entire frame.
Input chroma format.
Input frame height.
Input frame width.
Pitch. If set to zero, imageWidth is used; else, this field (assuming it's larger than imageWidth) is used.
Header generation mode.
Quality factor for encoder. Set to a value between 0 (lowest quality) and 100 (highest quality).