#include <ividtranscode.h>
Collaboration diagram for IVIDTRANSCODE_OutArgs:
size
parameter.
The size
field must be correctly set by the caller.
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Extended error information.
The value of each enum is the bit which is set.
Bits 31-16 are reserved. Bits 7-0 are codec and implementation specific.
The algorithm can set multiple bits to 1 based on conditions. e.g. it will set bits XDM_FATALERROR (fatal) and XDM_UNSUPPORTEDPARAM (unsupported params) in case of unsupported run time parameters.
This enumeration data type should not be used for storage, but rather only for its constant values.
Number of bits consumed during the IVIDTRANSCODE_Fxns.process() call.
Number of bits generated during the IVIDTRANSCODE_Fxns.process() call for each transcode output.
Decoded frame height
Decoded frame width
This is the ID of the encoded buffer for each output. This field is also used by the client to identify the outBufs
supplied with the IVIDTRANSCODE_Fxns.process() call that can be reused.
Flag to indicate if the current frame was skipped in specific transcode outputs.
When outputID
for a specific transcode output is non-zero, the corresponding encoded buffer related information is populated here.
Flag to indicate that the outBufs
provided with the IVIDTRANSCODE_Fxns.process() call are in use. No outBufs are required to be supplied with the next IVIDTRANSCODE_Fxns.process() call.