IVIDTRANSCODE_InArgs Struct Reference
[XDM IVIDTRANSCODE Video Transcoder Interface]

#include <ividtranscode.h>


Detailed Description

Defines the input arguments for all IVIDTRANSCODE instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.

The size field must be correctly set by the caller.

See also:
IVIDTRANSCODE_Fxns::process()


Data Fields

XDAS_Int32 size
XDAS_Int32 numBytes
XDAS_Int32 inputID


Field Documentation

XDAS_Int32 IVIDTRANSCODE_InArgs::size

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

XDAS_Int32 IVIDTRANSCODE_InArgs::numBytes

Size of input data in bytes, provided to the algorithm for decoding.

XDAS_Int32 IVIDTRANSCODE_InArgs::inputID

The decoder will attach this ID with the corresponding output frames.


The documentation for this struct was generated from the following file:
Copyright 2009, Texas Instruments Incorporated