#include <ividanalytics.h>
Collaboration diagram for IVIDANALYTICS_DynamicParams:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size
parameter.
The size
field must be correctly set by the caller.
Data Fields | |
XDAS_Int32 | size |
IVIDANALYTICS_Grid * | grid |
XDM_Date | date |
IVIDANALYTICS_Rule | rule |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
New overlay grid with analytics enable mask
Set the current time.
Rule associated with this command (if applicable).