IVIDANALYTICS_Rule Struct Reference
[XDM Beta Video Analytics Interface]

#include <ividanalytics.h>


Detailed Description

Analytics rule.


Data Fields

XDAS_Int32 size
XDAS_Int32 id
IVIDANALYTICS_ObjectType objectType
IVIDANALYTICS_ActionType actionType


Field Documentation

XDAS_Int32 IVIDANALYTICS_Rule::size

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

XDAS_Int32 IVIDANALYTICS_Rule::id

id associated with this rule.

IVIDANALYTICS_ObjectType IVIDANALYTICS_Rule::objectType

Type of the object associated with this rule.

IVIDANALYTICS_ActionType IVIDANALYTICS_Rule::actionType

Type of action associated with this rule.


The documentation for this struct was generated from the following file:
Copyright 2009, Texas Instruments Incorporated