ISPHENC_OutArgs Struct Reference
[XDM ISPHENC Speech/Voice Encoder Interface]

#include <isphenc.h>


Detailed Description

Defines the run time output arguments for all ISPHENC instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.

The size field must be correctly set by the caller.

See also:
ISPHENC_Fxns::process()


Data Fields

XDAS_Int32 size
XDAS_Int32 rate
XDAS_Int32 frameType
XDAS_Int32 outbufferSize


Field Documentation

XDAS_Int32 ISPHENC_OutArgs::size

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

XDAS_Int32 ISPHENC_OutArgs::rate

Current frame bit rate.

XDAS_Int32 ISPHENC_OutArgs::frameType

Current frame type.

XDAS_Int32 ISPHENC_OutArgs::outbufferSize

Output buffer size in bytes.


The documentation for this struct was generated from the following file:
Copyright 2009, Texas Instruments Incorporated