IIMGDEC1_InArgs Struct Reference
[XDM IIMGDEC1 Image Decoder Interface]

#include <iimgdec1.h>


Detailed Description

Defines the input arguments for all IIMGDEC1 instance process() function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.

The size field must be correctly set by the caller.

See also:
IIMGDEC1_Fxns::process()


Data Fields

XDAS_Int32 size
XDAS_Int32 numBytes


Field Documentation

XDAS_Int32 IIMGDEC1_InArgs::size

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

XDAS_Int32 IIMGDEC1_InArgs::numBytes

Size of input data in bytes, provided to the algorithm for decoding.


The documentation for this struct was generated from the following file:
Copyright 2009, Texas Instruments Incorporated