XDM IIMGDEC1 Image Decoder Interface


Detailed Description

This is the XDM IIMGDEC1 Image Decoder Interface.


Data Structures

struct  IIMGDEC1_Obj
 This must be the first field of all IIMGDEC1 instance objects. More...
struct  IIMGDEC1_Params
 Defines the creation time parameters for all IIMGDEC1 instance objects. More...
struct  IIMGDEC1_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls. More...
struct  IIMGDEC1_InArgs
 Defines the input arguments for all IIMGDEC1 instance process() function. More...
struct  IIMGDEC1_Status
 Defines instance status parameters. More...
struct  IIMGDEC1_OutArgs
 Defines the run time output arguments for all IIMGDEC1 instance objects. More...
struct  IIMGDEC1_Fxns
 Defines all of the operations on IIMGDEC1 objects. More...

Defines

#define IIMGDEC1_EOK   XDM_EOK
#define IIMGDEC1_EFAIL   XDM_EFAIL
#define IIMGDEC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Typedefs

typedef IIMGDEC1_ObjIIMGDEC1_Handle
 Opaque handle to an IIMGDEC1 objects.
typedef IALG_Cmd IIMGDEC1_Cmd
 Defines the control commands for the IIMGDEC1 module.


Define Documentation

#define IIMGDEC1_EOK   XDM_EOK

Success.

#define IIMGDEC1_EFAIL   XDM_EFAIL

General failure.

#define IIMGDEC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Request is unsupported.


Typedef Documentation

typedef struct IIMGDEC1_Obj* IIMGDEC1_Handle

Opaque handle to an IIMGDEC1 objects.

typedef IALG_Cmd IIMGDEC1_Cmd

Defines the control commands for the IIMGDEC1 module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId

IIMGDEC1_Fxns::control()


Copyright 2009, Texas Instruments Incorporated