#include <iimgdec1.h>
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size
parameter.
The size
field must be correctly set by the caller.
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | numAU |
XDAS_Int32 | decodeHeader |
XDAS_Int32 | displayWidth |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Number of Access unit to decode. Set to XDM_DEFAULT to decode the entire frame.
Decode entire access unit or only header.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
Pitch. If set to zero, imageWidth is used; else, this field (assuming it's larger than imageWidth) is used.