IAUDDEC1_Params Struct Reference
[XDM IAUDDEC1 Audio Decoder Interface]

#include <iauddec1.h>


Detailed Description

Defines the creation time parameters for all IAUDDEC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.

The size field must be correctly set by the caller.


Data Fields

XDAS_Int32 size
XDAS_Int32 outputPCMWidth
XDAS_Int32 pcmFormat
XDAS_Int32 dataEndianness


Field Documentation

XDAS_Int32 IAUDDEC1_Params::size

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

XDAS_Int32 IAUDDEC1_Params::outputPCMWidth

Number of bits per output PCM Sample.

XDAS_Int32 IAUDDEC1_Params::pcmFormat

Output PCM Format Block/Interleaved.

See also:
IAUDIO_PcmFormat

XDAS_Int32 IAUDDEC1_Params::dataEndianness

Endianness of output data.

See also:
XDM_DataFormat


The documentation for this struct was generated from the following file:
Copyright 2009, Texas Instruments Incorporated