XDM IAUDDEC1 Audio Decoder Interface


Detailed Description

This is the XDM IAUDDEC1 Audio Decoder Interface.


Data Structures

struct  IAUDDEC1_Obj
 This must be the first field of all IAUDDEC1 instance objects. More...
struct  IAUDDEC1_Params
 Defines the creation time parameters for all IAUDDEC1 instance objects. More...
struct  IAUDDEC1_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls. More...
struct  IAUDDEC1_InArgs
 Defines the input arguments for all IAUDDEC1 instance process function. More...
struct  IAUDDEC1_Status
 Defines instance status parameters (read-only). More...
struct  IAUDDEC1_OutArgs
 Defines the run time output arguments for all IAUDDEC1 instance objects. More...
struct  IAUDDEC1_Fxns
 Defines all of the operations on IAUDDEC1 objects. More...

Defines

#define IAUDDEC1_EOK   XDM_EOK
#define IAUDDEC1_EFAIL   XDM_EFAIL
#define IAUDDEC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Typedefs

typedef IAUDDEC1_ObjIAUDDEC1_Handle
 Opaque handle to an IAUDDEC1 objects.
typedef IALG_Cmd IAUDDEC1_Cmd
 Defines the control commands for the IAUDDEC1 module.


Define Documentation

#define IAUDDEC1_EOK   XDM_EOK

Success.

#define IAUDDEC1_EFAIL   XDM_EFAIL

General failure.

#define IAUDDEC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Request is unsupported.


Typedef Documentation

typedef struct IAUDDEC1_Obj* IAUDDEC1_Handle

Opaque handle to an IAUDDEC1 objects.

typedef IALG_Cmd IAUDDEC1_Cmd

Defines the control commands for the IAUDDEC1 module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId

IAUDDEC1_Fxns::control()


Copyright 2009, Texas Instruments Incorporated