#include <iauddec1.h>
size
parameter.
The size
field must be correctly set by the caller.
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | numBytes |
XDAS_Int32 | desiredChannelMode |
XDAS_Int32 | lfeFlag |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Size of input data in bytes, provided to the algorithm for decoding.
Flag indicating whether LFE channel data is desired in the output.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.