IAUDDEC1_DynamicParams Struct Reference
[XDM IAUDDEC1 Audio Decoder Interface]

#include <iauddec1.h>


Detailed Description

This structure defines the codec parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.

This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.

The size field must be correctly set by the caller.

See also:
IAUDDEC1_Fxns::control()


Data Fields

XDAS_Int32 size
XDAS_Int32 downSampleSbrFlag


Field Documentation

XDAS_Int32 IAUDDEC1_DynamicParams::size

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

XDAS_Int32 IAUDDEC1_DynamicParams::downSampleSbrFlag

Flag to indicate downsampling for SBR.

Valid values for this field are XDAS_TRUE and XDAS_FALSE.


The documentation for this struct was generated from the following file:
Copyright 2009, Texas Instruments Incorporated