TI-RTOS Drivers
tidrivers_full_2_20_00_08
|
Watchdog hardware attributes for CC3200. More...
#include <WatchdogCC3200.h>
Data Fields | |
unsigned int | baseAddr |
unsigned int | intNum |
unsigned int | intPriority |
uint32_t | reloadValue |
Watchdog hardware attributes for CC3200.
intPriority is the Watchdog timer's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.drivers.ports interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
unsigned int WatchdogCC3200_HWAttrs::baseAddr |
Base adddress for Watchdog
unsigned int WatchdogCC3200_HWAttrs::intNum |
WDT interrupt number
unsigned int WatchdogCC3200_HWAttrs::intPriority |
WDT interrupt priority
uint32_t WatchdogCC3200_HWAttrs::reloadValue |
Reload value for Watchdog