48 #ifndef ti_drivers_i2s_I2SCC3200DMA__include
49 #define ti_drivers_i2s_I2SCC3200DMA__include
87 #define I2SCC3200DMA_CMD_SET_ZEROBUF_LEN I2S_CMD_RESERVED + 0
88 #define I2SCC3200DMA_CMD_SET_EMPTYBUF_LEN I2S_CMD_RESERVED + 1
93 #define I2SCC3200DMA_SET_ZEROBUF_LEN I2SCC3200DMA_CMD_SET_ZEROBUF_LEN
94 #define I2SCC3200DMA_SET_EMPTYBUF_LEN I2SCC3200DMA_CMD_SET_EMPTYBUF_LEN
98 #define I2SCC3200DMA_INDEX_INVALID 0xFF
101 #define I2SCC3200DMA_NUM_SERIAL_PINS 2
void I2SCC3200DMA_Params_init(I2SCC3200DMA_SerialPinParams *params)
Function to initialize the I2S_Params struct to its defaults.
Definition: I2SCC3200DMA.h:113
const I2S_FxnTable I2SCC3200DMA_fxnTable
struct I2SCC3200DMA_SerialPinParams I2SCC3200DMA_SerialPinParams
CC3200 specific I2S Parameters.
SemaphoreP_Handle readSem
Definition: I2SCC3200DMA.h:225
The definition of a I2S function table that contains the required set of functions to control a speci...
Definition: I2S.h:431
uint32_t baseAddr
Definition: I2SCC3200DMA.h:155
I2SCC3200DMA_DataSize dmaSize
Definition: I2SCC3200DMA.h:221
UDMACC3200_Handle dmaHandle
Definition: I2SCC3200DMA.h:242
#define I2SCC3200DMA_NUM_SERIAL_PINS
Definition: I2SCC3200DMA.h:101
unsigned long rxChannelIndex
Definition: I2SCC3200DMA.h:161
struct I2SCC3200DMA_Object * I2SCC3200DMA_Handle
uDMA driver implementation for CC3200.
List_List readActiveQueue
Definition: I2SCC3200DMA.h:245
unsigned long zeroWriteBufLength
Definition: I2SCC3200DMA.h:229
struct I2SCC3200DMA_SerialPinConfig I2SCC3200DMA_SerialPinConfig
CC3200 Serial Pin Configuration.
SemaphoreP_Handle writeSem
Definition: I2SCC3200DMA.h:224
unsigned long txChannelIndex
Definition: I2SCC3200DMA.h:163
unsigned char pinNumber
Definition: I2SCC3200DMA.h:171
CC3200 specific I2S Parameters.
Definition: I2SCC3200DMA.h:184
I2S_Callback readWriteCallback
Definition: I2SCC3200DMA.h:199
struct I2SCC3200DMA_Object I2SCC3200DMA_Object
I2SCC3200DMA Object.
I2S_BufDesc * CurrentWriteBufDesc
Definition: I2SCC3200DMA.h:236
I2SCC3200DMA Hardware attributes.
Definition: I2SCC3200DMA.h:153
List_List writeDoneQueue
Definition: I2SCC3200DMA.h:248
HwiP_Handle hwiHandle
Definition: I2SCC3200DMA.h:226
void * SemaphoreP_Handle
Opaque client reference to an instance of a SemaphoreP.
Definition: SemaphoreP.h:96
Semaphore module for the RTOS Porting Interface.
I2S buffer descriptor for issue/reclaim mode.
Definition: I2S.h:258
uint32_t intPriority
Definition: I2SCC3200DMA.h:159
uint32_t intNum
Definition: I2SCC3200DMA.h:157
struct I2SCC3200DMA_HWAttrs I2SCC3200DMA_HWAttrs
I2SCC3200DMA Hardware attributes.
uint16_t writeIndex
Definition: I2SCC3200DMA.h:219
uint32_t readWriteTimeout
Definition: I2SCC3200DMA.h:201
unsigned long emptyReadBufLength
Definition: I2SCC3200DMA.h:233
uint32_t operationMode
Definition: I2SCC3200DMA.h:213
I2S_DataMode
I2S mode settings.
Definition: I2S.h:291
bool opened
Definition: I2SCC3200DMA.h:212
I2SCC3200DMA_SerialPinVars serialPinVars[I2SCC3200DMA_NUM_SERIAL_PINS]
Definition: I2SCC3200DMA.h:216
List_List readDoneQueue
Definition: I2SCC3200DMA.h:246
I2SCC3200DMA_DataSize
I2SCC3200DMA data size is used to determine how to configure the DMA data transfers. This field is to be only used internally.
Definition: I2SCC3200DMA.h:111
Definition: I2SCC3200DMA.h:112
struct I2SCC3200DMA_SerialPinVars I2SCC3200DMA_SerialPinVars
I2SCC3200DMA Serial pin variables.
UDMACC3200 Global configuration.
Definition: UDMACC3200.h:135
I2S_DataMode readWriteMode
Definition: I2SCC3200DMA.h:197
I2S_SerInActiveConfig
I2S Serializer InActive state settings.
Definition: I2S.h:324
void(* I2S_Callback)(I2S_Handle, I2S_BufDesc *desc)
The definition of a callback function used by the I2S driver when used in I2S_MODE_CALLBACK.
Definition: I2S.h:283
I2S_BufDesc * CurrentReadBufDesc
Definition: I2SCC3200DMA.h:239
I2S_PinMode pinMode
Definition: I2SCC3200DMA.h:174
I2SCC3200DMA_SerialPinConfig serialPinConfig[I2SCC3200DMA_NUM_SERIAL_PINS]
Definition: I2SCC3200DMA.h:187
uint16_t readIndex
Definition: I2SCC3200DMA.h:218
List_List writeActiveQueue
Definition: I2SCC3200DMA.h:247
I2S_SerInActiveConfig inActiveConfig
Definition: I2SCC3200DMA.h:177
void * HwiP_Handle
Opaque client reference to an instance of a HwiP.
Definition: HwiP.h:66
I2S_PinMode
I2S serial pin mode.
Definition: I2S.h:335
I2SCC3200DMA Object.
Definition: I2SCC3200DMA.h:210
Hardware Interrupt module for the RTOS Porting Interface.
CC3200 Serial Pin Configuration.
Definition: I2SCC3200DMA.h:169
Linked List interface for use in drivers.
I2SCC3200DMA Serial pin variables.
Definition: I2SCC3200DMA.h:196