TI-RTOS Drivers
tidrivers_full_2_20_00_08
|
EMACSnow Driver.
============================================================================
The EMACSnow header file should be included in an application as follows:
Refer to EMAC.h for a complete description of APIs.
The EMACSnow driver produces log statements using the instrumented library. The following masks are used:
#include <stdint.h>
#include <ti/sysbios/knl/Swi.h>
#include <ti/sysbios/family/arm/m3/Hwi.h>
#include <ti/drivers/EMAC.h>
#include <ti/ndk/inc/stkmain.h>
Go to the source code of this file.
Data Structures | |
struct | EMACSnow_HWAttrs |
EMACSnow Hardware attributes. More... | |
struct | EMACSnow_Object |
EMACSnow Object. More... | |
Macros | |
#define | ti_sysbios_family_arm_m3_Hwi__nolocalnames |
#define | _INCLUDE_NIMU_CODE |
Typedefs | |
typedef struct EMACSnow_HWAttrs | EMACSnow_HWAttrs |
EMACSnow Hardware attributes. More... | |
typedef struct EMACSnow_Object | EMACSnow_Object |
EMACSnow Object. More... | |
Functions | |
void | EMACSnow_init (uint32_t index) |
This function initializes the EMACSnow driver. More... | |
bool | EMACSnow_isLinkUp (uint32_t index) |
This function sets the EMACSnow driver. More... | |
int | EMACSnow_NIMUInit (STKEVENT_Handle hEvent) |
This function is needed in the NIMUDeviceTable that is required by the NDK. More... | |
Variables | |
const EMAC_FxnTable | EMACSnow_fxnTable |
EMACSnow function table. More... | |
#define ti_sysbios_family_arm_m3_Hwi__nolocalnames |
#define _INCLUDE_NIMU_CODE |
typedef struct EMACSnow_HWAttrs EMACSnow_HWAttrs |
EMACSnow Hardware attributes.
intPriority is the EMAC peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.drivers.ports interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
typedef struct EMACSnow_Object EMACSnow_Object |
EMACSnow Object.
This structure should not be directly accessed. It is specified here to allow the application to supply the needed memory to the EMACSnow module.
void EMACSnow_init | ( | uint32_t | index | ) |
This function initializes the EMACSnow driver.
This function must be called before the NDK stack thread is started.
The EMACSnow_config structure must be present and initialized before this function is called.
bool EMACSnow_isLinkUp | ( | uint32_t | index | ) |
This function sets the EMACSnow driver.
This function returns if the link is up
int EMACSnow_NIMUInit | ( | STKEVENT_Handle | hEvent | ) |
This function is needed in the NIMUDeviceTable that is required by the NDK.
const EMAC_FxnTable EMACSnow_fxnTable |
EMACSnow function table.