52 #ifndef ti_drivers_emac_EMACSnow__include
53 #define ti_drivers_emac_EMACSnow__include
60 #include <ti/sysbios/knl/Swi.h>
61 #define ti_sysbios_family_arm_m3_Hwi__nolocalnames
62 #include <ti/sysbios/family/arm/m3/Hwi.h>
66 #ifndef _INCLUDE_NIMU_CODE
67 #define _INCLUDE_NIMU_CODE
69 #include <ti/ndk/inc/stkmain.h>
132 #undef ti_sysbios_family_arm_m3_Hwi__nolocalnames
EMACSnow Hardware attributes.
Definition: EMACSnow.h:87
uint8_t * macAddress
Definition: EMACSnow.h:91
EMAC Function table structure.
Definition: EMAC.h:161
unsigned int intPriority
Definition: EMACSnow.h:90
unsigned int baseAddr
Definition: EMACSnow.h:88
struct EMACSnow_Object EMACSnow_Object
EMACSnow Object.
bool EMACSnow_isLinkUp(uint32_t index)
This function sets the EMACSnow driver.
unsigned int intNum
Definition: EMACSnow.h:89
int EMACSnow_NIMUInit(STKEVENT_Handle hEvent)
This function is needed in the NIMUDeviceTable that is required by the NDK.
Hwi_Handle hwi
Definition: EMACSnow.h:103
EMACSnow Object.
Definition: EMACSnow.h:101
Swi_Handle swi
Definition: EMACSnow.h:102
struct EMACSnow_HWAttrs EMACSnow_HWAttrs
EMACSnow Hardware attributes.
void EMACSnow_init(uint32_t index)
This function initializes the EMACSnow driver.
const EMAC_FxnTable EMACSnow_fxnTable
EMACSnow function table.