TI-RTOS Drivers  tidrivers_c2000_2_16_00_08
Data Structures | Macros | Typedefs | Functions
USBMSCHFatFs.h File Reference

Detailed Description

USBMSCHFatFs driver interface.

============================================================================

The USBMSCHFatFs header file should be included in an application as follows:

Operation

The USBMSCHFatFs driver is a driver designed to hook into FatFs. It implements a set of functions that FatFs needs to call to perform basic block data transfers.

This driver is designed to work with the USB Library. Because it is running in host mode, we need to add protection when accessing the USB Library. A gate was added to prevent the task servicing the USB library to preempt any other task accessing the USB Library.

Once the driver has been opened, the application may used the FatFs APIs or the standard C runtime file I/O calls (fopen, fclose, etc...). Once the driver has been closed, ensure the application does NOT make any file I/O calls.

Opening the driver

params.servicePriority = somePriority;
handle = USBMSCHFatFs_open(someUSBMSCHFatFs_configIndexValue, &params);
if (!handle) {
System_printf("USBMSCHFatFs did not open");
}

Implementation

This module serves as the main interface for TI-RTOS applications. Its purpose is to redirect the module's APIs to specific peripheral implementations which are specified using a pointer to a USBMSCHFatFs_FxnTable.

The USBMSCHFatFs driver interface module is joined (at link time) to a NULL-terminated array of USBMSCHFatFs_Config data structures named USBMSCHFatFs_config. USBMSCHFatFs_config is implemented in the application with each entry being an instance of a USBMSCHFatFs peripheral. Each entry in USBMSCHFatFs_config contains a:

Instrumentation

The USBMSCHFatFs driver interface produces log statements if instrumentation is enabled.

Diagnostics Mask Log details
Diags_USER1 basic operations performed
Diags_USER2 detailed operations performed

#include <stddef.h>
#include <stdint.h>
#include <stdbool.h>
Include dependency graph for USBMSCHFatFs.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  USBMSCHFatFs_Params
 USBMSCHFatFs Parameters. More...
 
struct  USBMSCHFatFs_FxnTable
 The definition of a USBMSCHFatFs function table that contains the required set of functions to control a specific USBMSCHFatFs driver implementation. More...
 
struct  USBMSCHFatFs_Config
 USBMSCHFatFs Global configuration. More...
 

Macros

#define USBMSCHFatFs_CMD_RESERVED   32
 
#define USBMSCHFatFs_STATUS_RESERVED   -32
 
#define USBMSCHFatFs_STATUS_SUCCESS   0
 Successful status code returned by USBMSCHFatFs_control(). More...
 
#define USBMSCHFatFs_STATUS_ERROR   -1
 Generic error status code returned by USBMSCHFatFs_control(). More...
 
#define USBMSCHFatFs_STATUS_UNDEFINEDCMD   -2
 An error status code returned by USBMSCHFatFs_control() for undefined command codes. More...
 

Typedefs

typedef struct USBMSCHFatFs_ConfigUSBMSCHFatFs_Handle
 USBMSCHFatFs Handler. More...
 
typedef struct USBMSCHFatFs_Params USBMSCHFatFs_Params
 USBMSCHFatFs Parameters. More...
 
typedef void(* USBMSCHFatFs_InitFxn) (USBMSCHFatFs_Handle handle)
 A function pointer to a driver specific implementation of USBMSCHFatFs_init(). More...
 
typedef USBMSCHFatFs_Handle(* USBMSCHFatFs_OpenFxn) (USBMSCHFatFs_Handle handle, unsigned char drv, USBMSCHFatFs_Params *params)
 A function pointer to a driver specific implementation of USBMSCHFatFs_open(). More...
 
typedef void(* USBMSCHFatFs_CloseFxn) (USBMSCHFatFs_Handle handle)
 A function pointer to a driver specific implementation of USBMSCHFatFs_close(). More...
 
typedef int(* USBMSCHFatFs_ControlFxn) (USBMSCHFatFs_Handle handle, unsigned int cmd, void *arg)
 A function pointer to a driver specific implementation of USBMSCHFatFs_control(). More...
 
typedef bool(* USBMSCHFatFs_waitForconnectFxn) (USBMSCHFatFs_Handle handle, unsigned int timeout)
 A function pointer to a driver specific implementation of USBMSCHFatFs_waitForConnect(). More...
 
typedef struct USBMSCHFatFs_FxnTable USBMSCHFatFs_FxnTable
 The definition of a USBMSCHFatFs function table that contains the required set of functions to control a specific USBMSCHFatFs driver implementation. More...
 
typedef struct USBMSCHFatFs_Config USBMSCHFatFs_Config
 USBMSCHFatFs Global configuration. More...
 

Functions

void USBMSCHFatFs_close (USBMSCHFatFs_Handle handle)
 Function to closes a given USBMSCHFatFs peripheral specified by the USBMSCHFatFs handle. This function unmounts the file system mounted by USBMSCHFatFs_open and unregisters the USBMSCHFatFs driver from BIOS' FatFs module. More...
 
int USBMSCHFatFs_control (USBMSCHFatFs_Handle handle, unsigned int cmd, void *arg)
 Function performs implementation specific features on a given USBMSCHFatFs_Handle. More...
 
void USBMSCHFatFs_init (void)
 Function to initialize the USBMSCHFatFs module. More...
 
USBMSCHFatFs_Handle USBMSCHFatFs_open (unsigned int index, unsigned char drv, USBMSCHFatFs_Params *params)
 This function registers the USBMSCHFatFs driver with BIOS' FatFs module and mounts the FatFs file system. More...
 
void USBMSCHFatFs_Params_init (USBMSCHFatFs_Params *params)
 Function to initialize the USBMSCHFatFs_Params structure to its defaults. More...
 
bool USBMSCHFatFs_waitForConnect (USBMSCHFatFs_Handle handle, unsigned int timeout)
 Function blocks task execution while no USB drive is enumerated. After the USBMSCHFatFs driver has been opened this functino is used to determine when a USB drive is has been enumerated. More...
 

Typedef Documentation

USBMSCHFatFs Handler.

USBMSCHFatFs Parameters.

USBMSCHFatFs parameters are used to with the USBMSCHFatFs_open() call. Default values for these parameters are set using USBMSCHFatFs_Params_init().

See also
USBMSCHFatFs_Params_init()
typedef void(* USBMSCHFatFs_InitFxn) (USBMSCHFatFs_Handle handle)

A function pointer to a driver specific implementation of USBMSCHFatFs_init().

typedef USBMSCHFatFs_Handle(* USBMSCHFatFs_OpenFxn) (USBMSCHFatFs_Handle handle, unsigned char drv, USBMSCHFatFs_Params *params)

A function pointer to a driver specific implementation of USBMSCHFatFs_open().

typedef void(* USBMSCHFatFs_CloseFxn) (USBMSCHFatFs_Handle handle)

A function pointer to a driver specific implementation of USBMSCHFatFs_close().

typedef int(* USBMSCHFatFs_ControlFxn) (USBMSCHFatFs_Handle handle, unsigned int cmd, void *arg)

A function pointer to a driver specific implementation of USBMSCHFatFs_control().

typedef bool(* USBMSCHFatFs_waitForconnectFxn) (USBMSCHFatFs_Handle handle, unsigned int timeout)

A function pointer to a driver specific implementation of USBMSCHFatFs_waitForConnect().

The definition of a USBMSCHFatFs function table that contains the required set of functions to control a specific USBMSCHFatFs driver implementation.

USBMSCHFatFs Global configuration.

The USBMSCHFatFs_Config structure contains a set of pointers used to characterize the USBMSCHFatFs driver implementation.

This structure needs to be defined before calling USBMSCHFatFs_init() and it must not be changed thereafter.

See also
USBMSCHFatFs_init()

Function Documentation

void USBMSCHFatFs_close ( USBMSCHFatFs_Handle  handle)

Function to closes a given USBMSCHFatFs peripheral specified by the USBMSCHFatFs handle. This function unmounts the file system mounted by USBMSCHFatFs_open and unregisters the USBMSCHFatFs driver from BIOS' FatFs module.

Precondition
USBMSCHFatFs_open() had to be called first.
Postcondition
After calling this function, it is safe to remove the USB drive
Parameters
handleA USBMSCHFatFs_Handle returned from USBMSCHFatFs_open
See also
USBMSCHFatFs_open()
int USBMSCHFatFs_control ( USBMSCHFatFs_Handle  handle,
unsigned int  cmd,
void *  arg 
)

Function performs implementation specific features on a given USBMSCHFatFs_Handle.

Commands for USBMSCHFatFs_control can originate from USBMSCHFatFs.h or from implementation specific USBMSCHFatFs*.h (USBMSCHFatFsTiva.h, etc.. ) files. While commands from USBMSCHFatFs.h are API portable across driver implementations, not all implementations may support all these commands. Conversely, commands from driver implementation specific USBMSCHFatFs*.h files add unique driver capabilities but are not API portable across all USBMSCHFatFs driver implementations.

Commands supported by USBMSCHFatFs.h follow a USBMSCHFatFs_CMD_<cmd> naming convention.
Commands supported by USBMSCHFatFs*.h follow a USBMSCHFatFs*_CMD_<cmd> naming convention.
Each control command defines arg differently. The types of arg are documented with each command.

See USBMSCHFatFs_control command codes for command codes.

See USBMSCHFatFs_control return status codes for status codes.

Precondition
USBMSCHFatFs_open() has to be called first.
Parameters
handleA USBMSCHFatFs handle returned from USBMSCHFatFs_open()
cmdUSBMSCHFatFs.h or USBMSCHFatFs*.h commands.
argAn optional R/W (read/write) command argument accompanied with cmd
Returns
Implementation specific return codes. Negative values indicate unsuccessful operations.
See also
USBMSCHFatFs_open()
void USBMSCHFatFs_init ( void  )

Function to initialize the USBMSCHFatFs module.

Precondition
The USBMSCHFatFs_config structure must exist and be persistent before this function can be called. This function must also be called before any other USBMSCHFatFs driver APIs. This function call does not modify any peripheral registers.
USBMSCHFatFs_Handle USBMSCHFatFs_open ( unsigned int  index,
unsigned char  drv,
USBMSCHFatFs_Params params 
)

This function registers the USBMSCHFatFs driver with BIOS' FatFs module and mounts the FatFs file system.

Precondition
USBMSCHFatFs_Params_init() has been called
Parameters
indexLogical peripheral number for the USBMSCHFatFs indexed into the USBMSCHFatFs_config table
drvDrive number to be associated with the USBMSCHFatFs FatFs driver
paramsPointer to an parameter block, if NULL it will use default values. All the fields in this structure are RO (read-only).
Returns
A pointer to a USBMSCHFatFs_Handle on success or a NULL it was already opened
See also
USBMSCHFatFs_init()
USBMSCHFatFs_close()
void USBMSCHFatFs_Params_init ( USBMSCHFatFs_Params params)

Function to initialize the USBMSCHFatFs_Params structure to its defaults.

Parameters
paramsAn pointer to USBMSCHFatFs_Params structure for initialization

Defaults values are: servicePriority = Task_numPriorities - 1;

bool USBMSCHFatFs_waitForConnect ( USBMSCHFatFs_Handle  handle,
unsigned int  timeout 
)

Function blocks task execution while no USB drive is enumerated. After the USBMSCHFatFs driver has been opened this functino is used to determine when a USB drive is has been enumerated.

Parameters
handleA USBMSCHFatFs handle
timeoutTimeout period in system ticks for the task to block
Returns
status:
  • true: Successful
  • false: timed out
Copyright 2016, Texas Instruments Incorporated