TI-RTOS for TivaC  2.14.04.31
Data Structures | Macros | Typedefs
GPIOMSP432.h File Reference

Detailed Description

MSP432 GPIO driver.

============================================================================

The GPIO header file should be included in an application as follows:

Operation

The GPIO module allows you to manage General Purpose I/O pins via simple and portable APIs. The application needs to supply a GPIOMSP432_Config structure to the module (see example below). This structure communicates to the GPIO module how to configure the pins used by the application (See the description of GPIO_PinConfig in the GPIO.h file).

The application is required to call GPIO_init(). This function will initialize all the GPIO pins defined in the GPIO_PinConfig table to the configurations specified. Once completed the other APIs can be used to access the pins.

Asserts are used to verify that the driver has only been initialized, and is reading/writing a valid index.

The following is an example of the code required to use the 2 switches and 4 LEDs on the MSP432 Launchpad board.

Board header:

// Enum of GPIO names on the MSP_EXP432P401R dev board
typedef enum MSP_EXP432P401R_GPIOName {
// input pins with callbacks first
MSP_EXP432P401R_S1 = 0,
MSP_EXP432P401R_S2,
// output pins
MSP_EXP432P401R_LED1,
MSP_EXP432P401R_LED_RED,
MSP_EXP432P401R_LED_GREEN,
MSP_EXP432P401R_LED_BLUE,
MSP_EXP432P401R_GPIOCOUNT
} MSP_EXP432P401R_GPIOName;

Board initialization code:

// Array of Pin configurations
// NOTE: The order of the pin configurations must coincide with what was
// defined in MSP_EXP432P401R.h
// NOTE: Pins not used for interrupts should be placed at the end of the
array. Callback entries can be omitted from callbacks array to
reduce memory usage.
const GPIO_PinConfig gpioPinConfigs[] = {
// Input pins
// MSP_EXP432P401R_S1
// MSP_EXP432P401R_S2
// Output pins
// MSP_EXP432P401R_LED1
// MSP_EXP432P401R_LED_RED
// MSP_EXP432P401R_LED_GREEN
// MSP_EXP432P401R_LED_BLUE
};
// Array of callback function pointers
// NOTE: The order of the pin configurations must coincide with what was
// defined in MSP_EXP432P401R.h
// NOTE: Pins not used for interrupts can be omitted from callbacks array to
reduce memory usage (if placed at end of gpioPinConfigs array).
const GPIO_callbackFxn gpioCallbackFunctions[] = {
// MSP_EXP432P401R_S1
NULL,
// MSP_EXP432P401R_S2
NULL
};
//
// The device-specific GPIO_config structure
//
const GPIOMSP432_Config GPIOMSP432_config = {
.pinConfigs = (GPIO_PinConfig *)gpioPinConfigs,
.callbacks = (GPIO_CallbackFxn *)gpioCallbackFunctions,
.numberOfPinConfigs =
sizeof(gpioPinConfigs)/sizeof(GPIO_PinConfig),
.numberOfCallbacks =
sizeof(gpioCallbackFunctions)/sizeof(GPIO_CallbackFxn),
.intPriority = (~0)
};
// Initialize peripheral and pins
void MSP_EXP432P401R_initGPIO(void)
{
// set up initial GPIO pin configurations
}

Keep in mind that the callback functions will be called in the context of an interrupt service routine and should be designed accordingly. When an interrupt is triggered, the interrupt status of all (interrupt enabled) pins on a port will be read, cleared, and the respective callbacks will be executed. Callbacks will be called in order from least significant bit to most significant bit.

Instrumentation

The GPIO driver interface produces log statements if instrumentation is enabled.

Diagnostics Mask Log details
Diags_USER1 basic operations performed

#include <stdint.h>
#include <ti/drivers/GPIO.h>
Include dependency graph for GPIOMSP432.h:

Go to the source code of this file.

Data Structures

struct  GPIOMSP432_Config
 GPIO device specific driver configuration structure. More...
 

Macros

#define GPIOMSP432_EMPTY_PIN   0x0000
 Device specific port/pin definition macros. More...
 
#define GPIOMSP432_P1_0   0x101
 
#define GPIOMSP432_P1_1   0x102
 
#define GPIOMSP432_P1_2   0x104
 
#define GPIOMSP432_P1_3   0x108
 
#define GPIOMSP432_P1_4   0x110
 
#define GPIOMSP432_P1_5   0x120
 
#define GPIOMSP432_P1_6   0x140
 
#define GPIOMSP432_P1_7   0x180
 
#define GPIOMSP432_P2_0   0x201
 
#define GPIOMSP432_P2_1   0x202
 
#define GPIOMSP432_P2_2   0x204
 
#define GPIOMSP432_P2_3   0x208
 
#define GPIOMSP432_P2_4   0x210
 
#define GPIOMSP432_P2_5   0x220
 
#define GPIOMSP432_P2_6   0x240
 
#define GPIOMSP432_P2_7   0x280
 
#define GPIOMSP432_P3_0   0x301
 
#define GPIOMSP432_P3_1   0x302
 
#define GPIOMSP432_P3_2   0x304
 
#define GPIOMSP432_P3_3   0x308
 
#define GPIOMSP432_P3_4   0x310
 
#define GPIOMSP432_P3_5   0x320
 
#define GPIOMSP432_P3_6   0x340
 
#define GPIOMSP432_P3_7   0x380
 
#define GPIOMSP432_P4_0   0x401
 
#define GPIOMSP432_P4_1   0x402
 
#define GPIOMSP432_P4_2   0x404
 
#define GPIOMSP432_P4_3   0x408
 
#define GPIOMSP432_P4_4   0x410
 
#define GPIOMSP432_P4_5   0x420
 
#define GPIOMSP432_P4_6   0x440
 
#define GPIOMSP432_P4_7   0x480
 
#define GPIOMSP432_P5_0   0x501
 
#define GPIOMSP432_P5_1   0x502
 
#define GPIOMSP432_P5_2   0x504
 
#define GPIOMSP432_P5_3   0x508
 
#define GPIOMSP432_P5_4   0x510
 
#define GPIOMSP432_P5_5   0x520
 
#define GPIOMSP432_P5_6   0x540
 
#define GPIOMSP432_P5_7   0x580
 
#define GPIOMSP432_P6_0   0x601
 
#define GPIOMSP432_P6_1   0x602
 
#define GPIOMSP432_P6_2   0x604
 
#define GPIOMSP432_P6_3   0x608
 
#define GPIOMSP432_P6_4   0x610
 
#define GPIOMSP432_P6_5   0x620
 
#define GPIOMSP432_P6_6   0x640
 
#define GPIOMSP432_P6_7   0x680
 
#define GPIOMSP432_P7_0   0x701
 
#define GPIOMSP432_P7_1   0x702
 
#define GPIOMSP432_P7_2   0x704
 
#define GPIOMSP432_P7_3   0x708
 
#define GPIOMSP432_P7_4   0x710
 
#define GPIOMSP432_P7_5   0x720
 
#define GPIOMSP432_P7_6   0x740
 
#define GPIOMSP432_P7_7   0x780
 
#define GPIOMSP432_P8_0   0x801
 
#define GPIOMSP432_P8_1   0x802
 
#define GPIOMSP432_P8_2   0x804
 
#define GPIOMSP432_P8_3   0x808
 
#define GPIOMSP432_P8_4   0x810
 
#define GPIOMSP432_P8_5   0x820
 
#define GPIOMSP432_P8_6   0x840
 
#define GPIOMSP432_P8_7   0x880
 
#define GPIOMSP432_P9_0   0x901
 
#define GPIOMSP432_P9_1   0x902
 
#define GPIOMSP432_P9_2   0x904
 
#define GPIOMSP432_P9_3   0x908
 
#define GPIOMSP432_P9_4   0x910
 
#define GPIOMSP432_P9_5   0x920
 
#define GPIOMSP432_P9_6   0x940
 
#define GPIOMSP432_P9_7   0x980
 
#define GPIOMSP432_P10_0   0xa01
 
#define GPIOMSP432_P10_1   0xa02
 
#define GPIOMSP432_P10_2   0xa04
 
#define GPIOMSP432_P10_3   0xa08
 
#define GPIOMSP432_P10_4   0xa10
 
#define GPIOMSP432_P10_5   0xa20
 
#define GPIOMSP432_P10_6   0xa40
 
#define GPIOMSP432_P10_7   0xa80
 
#define GPIOMSP432_PJ_0   0xb01
 
#define GPIOMSP432_PJ_1   0xb02
 
#define GPIOMSP432_PJ_2   0xb04
 
#define GPIOMSP432_PJ_3   0xb08
 
#define GPIOMSP432_PJ_4   0xb10
 
#define GPIOMSP432_PJ_5   0xb20
 
#define GPIOMSP432_PJ_6   0xb40
 
#define GPIOMSP432_PJ_7   0xb80
 

Typedefs

typedef struct GPIOMSP432_Config GPIOMSP432_Config
 GPIO device specific driver configuration structure. More...
 

Macro Definition Documentation

#define GPIOMSP432_EMPTY_PIN   0x0000

Device specific port/pin definition macros.

Below are the port/pin definitions to be used within the board's pin configuration table. These macros should be or'd in with the respective pin configuration settings.

#define GPIOMSP432_P1_0   0x101
#define GPIOMSP432_P1_1   0x102
#define GPIOMSP432_P1_2   0x104
#define GPIOMSP432_P1_3   0x108
#define GPIOMSP432_P1_4   0x110
#define GPIOMSP432_P1_5   0x120
#define GPIOMSP432_P1_6   0x140
#define GPIOMSP432_P1_7   0x180
#define GPIOMSP432_P2_0   0x201
#define GPIOMSP432_P2_1   0x202
#define GPIOMSP432_P2_2   0x204
#define GPIOMSP432_P2_3   0x208
#define GPIOMSP432_P2_4   0x210
#define GPIOMSP432_P2_5   0x220
#define GPIOMSP432_P2_6   0x240
#define GPIOMSP432_P2_7   0x280
#define GPIOMSP432_P3_0   0x301
#define GPIOMSP432_P3_1   0x302
#define GPIOMSP432_P3_2   0x304
#define GPIOMSP432_P3_3   0x308
#define GPIOMSP432_P3_4   0x310
#define GPIOMSP432_P3_5   0x320
#define GPIOMSP432_P3_6   0x340
#define GPIOMSP432_P3_7   0x380
#define GPIOMSP432_P4_0   0x401
#define GPIOMSP432_P4_1   0x402
#define GPIOMSP432_P4_2   0x404
#define GPIOMSP432_P4_3   0x408
#define GPIOMSP432_P4_4   0x410
#define GPIOMSP432_P4_5   0x420
#define GPIOMSP432_P4_6   0x440
#define GPIOMSP432_P4_7   0x480
#define GPIOMSP432_P5_0   0x501
#define GPIOMSP432_P5_1   0x502
#define GPIOMSP432_P5_2   0x504
#define GPIOMSP432_P5_3   0x508
#define GPIOMSP432_P5_4   0x510
#define GPIOMSP432_P5_5   0x520
#define GPIOMSP432_P5_6   0x540
#define GPIOMSP432_P5_7   0x580
#define GPIOMSP432_P6_0   0x601
#define GPIOMSP432_P6_1   0x602
#define GPIOMSP432_P6_2   0x604
#define GPIOMSP432_P6_3   0x608
#define GPIOMSP432_P6_4   0x610
#define GPIOMSP432_P6_5   0x620
#define GPIOMSP432_P6_6   0x640
#define GPIOMSP432_P6_7   0x680
#define GPIOMSP432_P7_0   0x701
#define GPIOMSP432_P7_1   0x702
#define GPIOMSP432_P7_2   0x704
#define GPIOMSP432_P7_3   0x708
#define GPIOMSP432_P7_4   0x710
#define GPIOMSP432_P7_5   0x720
#define GPIOMSP432_P7_6   0x740
#define GPIOMSP432_P7_7   0x780
#define GPIOMSP432_P8_0   0x801
#define GPIOMSP432_P8_1   0x802
#define GPIOMSP432_P8_2   0x804
#define GPIOMSP432_P8_3   0x808
#define GPIOMSP432_P8_4   0x810
#define GPIOMSP432_P8_5   0x820
#define GPIOMSP432_P8_6   0x840
#define GPIOMSP432_P8_7   0x880
#define GPIOMSP432_P9_0   0x901
#define GPIOMSP432_P9_1   0x902
#define GPIOMSP432_P9_2   0x904
#define GPIOMSP432_P9_3   0x908
#define GPIOMSP432_P9_4   0x910
#define GPIOMSP432_P9_5   0x920
#define GPIOMSP432_P9_6   0x940
#define GPIOMSP432_P9_7   0x980
#define GPIOMSP432_P10_0   0xa01
#define GPIOMSP432_P10_1   0xa02
#define GPIOMSP432_P10_2   0xa04
#define GPIOMSP432_P10_3   0xa08
#define GPIOMSP432_P10_4   0xa10
#define GPIOMSP432_P10_5   0xa20
#define GPIOMSP432_P10_6   0xa40
#define GPIOMSP432_P10_7   0xa80
#define GPIOMSP432_PJ_0   0xb01
#define GPIOMSP432_PJ_1   0xb02
#define GPIOMSP432_PJ_2   0xb04
#define GPIOMSP432_PJ_3   0xb08
#define GPIOMSP432_PJ_4   0xb10
#define GPIOMSP432_PJ_5   0xb20
#define GPIOMSP432_PJ_6   0xb40
#define GPIOMSP432_PJ_7   0xb80

Typedef Documentation

GPIO device specific driver configuration structure.

Copyright 2015, Texas Instruments Incorporated