TI-RTOS for TivaC  2.14.04.31
Data Structures | Macros | Typedefs
GPIOMSP430.h File Reference

Detailed Description

MSP430 GPIO driver.

============================================================================

The GPIO header file should be included in an application as follows:

Operation

The GPIO module allows you to manage General Purpose I/O pins via simple and portable APIs. The application is required to supply a GPIOMSP430_Config structure to the module (see example below). This structure communicates to the GPIO module how to configure the pins used by the application (See the description of GPIO_PinConfig in the GPIO.h file).

The application is required to call GPIO_init(). This function will initialize all the GPIO pins defined in the GPIO_PinConfig table to the configurations specified. Once completed the other APIs can be used to access the pins.

Asserts are used to verify that the driver has been initialized, and is reading/writing a valid index.

The following is an example of the code required to use 2 switches and 2 LEDs on an MSP_EXP430F5529 Launchpad board.

Board header file:

// Enum of GPIO names on the MSP_EXP430F5529LP dev board
typedef enum MSP_EXP430F5529LP_GPIOName {
MSP_EXP430F5529LP_S1 = 0,
MSP_EXP430F5529LP_S2,
MSP_EXP430F5529LP_LED1,
MSP_EXP430F5529LP_LED2,
MSP_EXP430F5529LP_GPIOCOUNT
} MSP_EXP430F5529LP_GPIOName;

Board initialization code:

// Array of pin configurations
// NOTE: The order of the pin configurations must coincide with what was
// defined in MSP_EXP4305529LP.h
// NOTE: Pins not used for interrupts should be placed at the end of the
// array. Callback entries can be omitted from callbacks array to
// reduce memory usage.
const GPIO_PinConfig gpioPinConfigs[] = {
// Input pins
// MSP_EXP430F5529LP_S1
// MSP_EXP430F5529LP_S2
// Output pins
// MSP_EXP430F5529LP_LED1
// MSP_EXP430F5529LP_LED2
};
// Array of callback function pointers
// NOTE: The order of the pin configurations must coincide with what was
// defined in MSP_EXP4305529LP.h
// NOTE: Pins not used for interrupts can be omitted from callbacks array to
// reduce memory usage (if placed at end of gpioPinConfigs array).
const GPIO_callbackFxn gpioCallbackFunctions[] = {
NULL, // MSP_EXP430F5529LP_S1
NULL // MSP_EXP430F5529LP_S2
};
// The device-specific GPIO_config structure
const GPIOMSP430_Config GPIOMSP430_config = {
.pinConfigs = (GPIO_PinConfig *) gpioPinConfigs,
.callbacks = (GPIO_CallbackFxn *) gpioCallbackFunctions,
.numberOfPinConfigs = sizeof(gpioPinConfigs) / sizeof(GPIO_PinConfig),
.numberOfCallbacks = sizeof(gpioCallbackFunctions) / sizeof(GPIO_CallbackFxn)
};
// Initialize peripheral and pins
void MSP_EXP430F5529LP_initGPIO(void)
{
}

MSP430 devices require GPIO interrupts to be statically created in the application specific configuration. The interrupt service routine for the Hwi must be set to "GPIO_hwiIntFxn". Additionally, the GPIO port number must be provided as a Hwi parameter. When an interrupt is triggered, the interrupt status of all (interrupt enabled) pins on a port will be read, cleared, and the respective callbacks will be executed. Callbacks will be called in order from least significant bit to most significant bit. Keep in mind that the callback functions will be called in the context of an interrupt service routine and should be designed accordingly. The following is an example for creating a Hwi for Port 2.

Application configuration file:

// All Hwis must be created statically; including those for TI-RTOS drivers.
var hwiParams = new Hwi.Params();
// Add the GPIO port number as a Hwi argument.
hwiParams.arg = 2;
// Create the Hwi with GPIO Port interrupt number and using GPIO_hwiIntFxn
// as the Hwi function.
Program.global.hwi0 = Hwi.create(42, "&GPIO_hwiIntFxn", hwiParams);

Callback functions can be assigned to interrupt enabled input pins on Port 2.

Instrumentation

The GPIO driver interface produces log statements if instrumentation is enabled.

Diagnostics Mask Log details
Diags_USER1 basic operations performed

#include <stdint.h>
#include <ti/drivers/GPIO.h>
Include dependency graph for GPIOMSP430.h:

Go to the source code of this file.

Data Structures

struct  GPIOMSP430_Config
 GPIO device specific driver configuration structure. More...
 

Macros

#define GPIOMSP430_EMPTY_PIN   0x0000
 Device specific port/pin definition macros. More...
 
#define GPIOMSP430_P1_0   0x0101
 
#define GPIOMSP430_P1_1   0x0102
 
#define GPIOMSP430_P1_2   0x0104
 
#define GPIOMSP430_P1_3   0x0108
 
#define GPIOMSP430_P1_4   0x0110
 
#define GPIOMSP430_P1_5   0x0120
 
#define GPIOMSP430_P1_6   0x0140
 
#define GPIOMSP430_P1_7   0x0180
 
#define GPIOMSP430_P2_0   0x0201
 
#define GPIOMSP430_P2_1   0x0202
 
#define GPIOMSP430_P2_2   0x0204
 
#define GPIOMSP430_P2_3   0x0208
 
#define GPIOMSP430_P2_4   0x0210
 
#define GPIOMSP430_P2_5   0x0220
 
#define GPIOMSP430_P2_6   0x0240
 
#define GPIOMSP430_P2_7   0x0280
 
#define GPIOMSP430_P3_0   0x0301
 
#define GPIOMSP430_P3_1   0x0302
 
#define GPIOMSP430_P3_2   0x0304
 
#define GPIOMSP430_P3_3   0x0308
 
#define GPIOMSP430_P3_4   0x0310
 
#define GPIOMSP430_P3_5   0x0320
 
#define GPIOMSP430_P3_6   0x0340
 
#define GPIOMSP430_P3_7   0x0380
 
#define GPIOMSP430_P4_0   0x0401
 
#define GPIOMSP430_P4_1   0x0402
 
#define GPIOMSP430_P4_2   0x0404
 
#define GPIOMSP430_P4_3   0x0408
 
#define GPIOMSP430_P4_4   0x0410
 
#define GPIOMSP430_P4_5   0x0420
 
#define GPIOMSP430_P4_6   0x0440
 
#define GPIOMSP430_P4_7   0x0480
 
#define GPIOMSP430_P5_0   0x0501
 
#define GPIOMSP430_P5_1   0x0502
 
#define GPIOMSP430_P5_2   0x0504
 
#define GPIOMSP430_P5_3   0x0508
 
#define GPIOMSP430_P5_4   0x0510
 
#define GPIOMSP430_P5_5   0x0520
 
#define GPIOMSP430_P5_6   0x0540
 
#define GPIOMSP430_P5_7   0x0580
 
#define GPIOMSP430_P6_0   0x0601
 
#define GPIOMSP430_P6_1   0x0602
 
#define GPIOMSP430_P6_2   0x0604
 
#define GPIOMSP430_P6_3   0x0608
 
#define GPIOMSP430_P6_4   0x0610
 
#define GPIOMSP430_P6_5   0x0620
 
#define GPIOMSP430_P6_6   0x0640
 
#define GPIOMSP430_P6_7   0x0680
 
#define GPIOMSP430_P7_0   0x0701
 
#define GPIOMSP430_P7_1   0x0702
 
#define GPIOMSP430_P7_2   0x0704
 
#define GPIOMSP430_P7_3   0x0708
 
#define GPIOMSP430_P7_4   0x0710
 
#define GPIOMSP430_P7_5   0x0720
 
#define GPIOMSP430_P7_6   0x0740
 
#define GPIOMSP430_P7_7   0x0780
 
#define GPIOMSP430_P8_0   0x0801
 
#define GPIOMSP430_P8_1   0x0802
 
#define GPIOMSP430_P8_2   0x0804
 
#define GPIOMSP430_P8_3   0x0808
 
#define GPIOMSP430_P8_4   0x0810
 
#define GPIOMSP430_P8_5   0x0820
 
#define GPIOMSP430_P8_6   0x0840
 
#define GPIOMSP430_P8_7   0x0880
 
#define GPIOMSP430_P9_0   0x0901
 
#define GPIOMSP430_P9_1   0x0902
 
#define GPIOMSP430_P9_2   0x0904
 
#define GPIOMSP430_P9_3   0x0908
 
#define GPIOMSP430_P9_4   0x0910
 
#define GPIOMSP430_P9_5   0x0920
 
#define GPIOMSP430_P9_6   0x0940
 
#define GPIOMSP430_P9_7   0x0980
 
#define GPIOMSP430_P10_0   0x0A01
 
#define GPIOMSP430_P10_1   0x0A02
 
#define GPIOMSP430_P10_2   0x0A04
 
#define GPIOMSP430_P10_3   0x0A08
 
#define GPIOMSP430_P10_4   0x0A10
 
#define GPIOMSP430_P10_5   0x0A20
 
#define GPIOMSP430_P10_6   0x0A40
 
#define GPIOMSP430_P10_7   0x0A80
 
#define GPIOMSP430_P11_0   0x0B01
 
#define GPIOMSP430_P11_1   0x0B02
 
#define GPIOMSP430_P11_2   0x0B04
 
#define GPIOMSP430_P11_3   0x0B08
 
#define GPIOMSP430_P11_4   0x0B10
 
#define GPIOMSP430_P11_5   0x0B20
 
#define GPIOMSP430_P11_6   0x0B40
 
#define GPIOMSP430_P11_7   0x0B80
 
#define GPIOMSP430_PJ_0   0x0D01
 
#define GPIOMSP430_PJ_1   0x0D02
 
#define GPIOMSP430_PJ_2   0x0D04
 
#define GPIOMSP430_PJ_3   0x0D08
 
#define GPIOMSP430_PJ_4   0x0D10
 
#define GPIOMSP430_PJ_5   0x0D20
 
#define GPIOMSP430_PJ_6   0x0D40
 
#define GPIOMSP430_PJ_7   0x0D80
 

Typedefs

typedef struct GPIOMSP430_Config GPIOMSP430_Config
 GPIO device specific driver configuration structure. More...
 

Macro Definition Documentation

#define GPIOMSP430_EMPTY_PIN   0x0000

Device specific port/pin definition macros.

Below are the port/pin definitions to be used within the board's pin configuration table.

#define GPIOMSP430_P1_0   0x0101
#define GPIOMSP430_P1_1   0x0102
#define GPIOMSP430_P1_2   0x0104
#define GPIOMSP430_P1_3   0x0108
#define GPIOMSP430_P1_4   0x0110
#define GPIOMSP430_P1_5   0x0120
#define GPIOMSP430_P1_6   0x0140
#define GPIOMSP430_P1_7   0x0180
#define GPIOMSP430_P2_0   0x0201
#define GPIOMSP430_P2_1   0x0202
#define GPIOMSP430_P2_2   0x0204
#define GPIOMSP430_P2_3   0x0208
#define GPIOMSP430_P2_4   0x0210
#define GPIOMSP430_P2_5   0x0220
#define GPIOMSP430_P2_6   0x0240
#define GPIOMSP430_P2_7   0x0280
#define GPIOMSP430_P3_0   0x0301
#define GPIOMSP430_P3_1   0x0302
#define GPIOMSP430_P3_2   0x0304
#define GPIOMSP430_P3_3   0x0308
#define GPIOMSP430_P3_4   0x0310
#define GPIOMSP430_P3_5   0x0320
#define GPIOMSP430_P3_6   0x0340
#define GPIOMSP430_P3_7   0x0380
#define GPIOMSP430_P4_0   0x0401
#define GPIOMSP430_P4_1   0x0402
#define GPIOMSP430_P4_2   0x0404
#define GPIOMSP430_P4_3   0x0408
#define GPIOMSP430_P4_4   0x0410
#define GPIOMSP430_P4_5   0x0420
#define GPIOMSP430_P4_6   0x0440
#define GPIOMSP430_P4_7   0x0480
#define GPIOMSP430_P5_0   0x0501
#define GPIOMSP430_P5_1   0x0502
#define GPIOMSP430_P5_2   0x0504
#define GPIOMSP430_P5_3   0x0508
#define GPIOMSP430_P5_4   0x0510
#define GPIOMSP430_P5_5   0x0520
#define GPIOMSP430_P5_6   0x0540
#define GPIOMSP430_P5_7   0x0580
#define GPIOMSP430_P6_0   0x0601
#define GPIOMSP430_P6_1   0x0602
#define GPIOMSP430_P6_2   0x0604
#define GPIOMSP430_P6_3   0x0608
#define GPIOMSP430_P6_4   0x0610
#define GPIOMSP430_P6_5   0x0620
#define GPIOMSP430_P6_6   0x0640
#define GPIOMSP430_P6_7   0x0680
#define GPIOMSP430_P7_0   0x0701
#define GPIOMSP430_P7_1   0x0702
#define GPIOMSP430_P7_2   0x0704
#define GPIOMSP430_P7_3   0x0708
#define GPIOMSP430_P7_4   0x0710
#define GPIOMSP430_P7_5   0x0720
#define GPIOMSP430_P7_6   0x0740
#define GPIOMSP430_P7_7   0x0780
#define GPIOMSP430_P8_0   0x0801
#define GPIOMSP430_P8_1   0x0802
#define GPIOMSP430_P8_2   0x0804
#define GPIOMSP430_P8_3   0x0808
#define GPIOMSP430_P8_4   0x0810
#define GPIOMSP430_P8_5   0x0820
#define GPIOMSP430_P8_6   0x0840
#define GPIOMSP430_P8_7   0x0880
#define GPIOMSP430_P9_0   0x0901
#define GPIOMSP430_P9_1   0x0902
#define GPIOMSP430_P9_2   0x0904
#define GPIOMSP430_P9_3   0x0908
#define GPIOMSP430_P9_4   0x0910
#define GPIOMSP430_P9_5   0x0920
#define GPIOMSP430_P9_6   0x0940
#define GPIOMSP430_P9_7   0x0980
#define GPIOMSP430_P10_0   0x0A01
#define GPIOMSP430_P10_1   0x0A02
#define GPIOMSP430_P10_2   0x0A04
#define GPIOMSP430_P10_3   0x0A08
#define GPIOMSP430_P10_4   0x0A10
#define GPIOMSP430_P10_5   0x0A20
#define GPIOMSP430_P10_6   0x0A40
#define GPIOMSP430_P10_7   0x0A80
#define GPIOMSP430_P11_0   0x0B01
#define GPIOMSP430_P11_1   0x0B02
#define GPIOMSP430_P11_2   0x0B04
#define GPIOMSP430_P11_3   0x0B08
#define GPIOMSP430_P11_4   0x0B10
#define GPIOMSP430_P11_5   0x0B20
#define GPIOMSP430_P11_6   0x0B40
#define GPIOMSP430_P11_7   0x0B80
#define GPIOMSP430_PJ_0   0x0D01
#define GPIOMSP430_PJ_1   0x0D02
#define GPIOMSP430_PJ_2   0x0D04
#define GPIOMSP430_PJ_3   0x0D08
#define GPIOMSP430_PJ_4   0x0D10
#define GPIOMSP430_PJ_5   0x0D20
#define GPIOMSP430_PJ_6   0x0D40
#define GPIOMSP430_PJ_7   0x0D80

Typedef Documentation

GPIO device specific driver configuration structure.

Copyright 2015, Texas Instruments Incorporated