Data Fields

RingIO_openParams_Tag Struct Reference

Structure defining config parameters for opening the RingIO instances. More...

#include <RingIO.h>

Data Fields

UInt32 flags
RingIO_OpenMode openMode

Detailed Description

Structure defining config parameters for opening the RingIO instances.


Field Documentation

Flags to set behavior of RingIO (e.g. cache maintenance, use exact size). See RingIO_Flags

Mode in which client will be opened


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated