Defines | Typedefs

Std.h File Reference


Detailed Description

This will have definitions of standard data types for platform abstraction.

Go to the source code of this file.

Defines

#define TRUE   1
#define FALSE   0
#define Error_init(eb)   *eb = 0

Typedefs

typedef char Char
typedef unsigned char UChar
typedef short Short
typedef unsigned short UShort
typedef int Int
typedef unsigned int UInt
typedef long Long
typedef unsigned long ULong
typedef float Float
typedef double Double
typedef long double LDouble
typedef void Void
typedef unsigned short Bool
typedef void * Ptr
typedef char * String
typedef int * IArg
typedef unsigned int * UArg
typedef char Int8
typedef short Int16
typedef int Int32
typedef unsigned char UInt8
typedef unsigned short UInt16
typedef unsigned int UInt32
typedef unsigned int SizeT
typedef unsigned char Bits8
typedef unsigned short Bits16
typedef UInt32 Bits32
typedef UInt32 Error_Block

Define Documentation

#define TRUE   1
#define FALSE   0
#define Error_init (   eb )    *eb = 0

Initialize error block


Typedef Documentation

typedef char Char
typedef unsigned char UChar
typedef short Short
typedef unsigned short UShort
typedef int Int
typedef unsigned int UInt
typedef long Long
typedef unsigned long ULong
typedef float Float
typedef double Double
typedef long double LDouble
typedef void Void
typedef unsigned short Bool
typedef void* Ptr
typedef char* String
typedef int* IArg
typedef unsigned int* UArg
typedef char Int8
typedef short Int16
typedef int Int32
typedef unsigned char UInt8
typedef unsigned short UInt16
typedef unsigned int UInt32
typedef unsigned int SizeT
typedef unsigned char Bits8
typedef unsigned short Bits16
typedef UInt32 Bits32

Data type for errors

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated