Data Fields

ProcMgr_MappedMemEntry Struct Reference

Structure containing information of mapped memory regions. More...

#include <ProcMgr.h>

Collaboration diagram for ProcMgr_MappedMemEntry:
Collaboration graph
[legend]

Data Fields

ProcMgr_AddrInfo info
ProcMgr_AddrType srcAddrType
ProcMgr_MapMask mapMask
Bool inUse

Detailed Description

Structure containing information of mapped memory regions.


Field Documentation

Address information

Source address type used for mapping

Mapping type

Entry index is in use?


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated