Structure defining notification parameter structure. More...
#include <FrameQBufMgr.h>
Data Fields | |
SysLink_NotifyType | notifyType |
UInt32 | watermark |
FrameQBufMgr_NotifyFunc | cbFxnPtr |
Ptr | cbContext |
Ptr | cbClientHandle |
Structure defining notification parameter structure.
SysLink_NotifyType FrameQBufMgr_NotifyParams_Tag::notifyType |
Notification type.See SysLink_NotifyType
Minumum number of free frames required to generate notification Same water mark for all the individual freeFramePools in the set.
Cacll back function
Context pointer that needs to be passed to call back function.
Handle that needs to be passed as first arg to call back. Ideally this should be callers client handle.