Data Fields

FrameQ_NotifyParams_Tag Struct Reference

Structure defining notification parameter structure. More...

#include <FrameQ.h>

Data Fields

FrameQ_NotifyType notifyType
UInt32 watermark
FrameQ_NotifyFunc cbFxnPtr
Ptr cbContext
Ptr cbClientHandle

Detailed Description

Structure defining notification parameter structure.


Field Documentation

Notification type

Minumum number of free frames required to generate notification Same water mark for all the individual freeFramePools in the set.

Cacll back function

Context pointer that needs to be passed to call back function.

Handle that needs to be passed as first arg to call back. Ideally this should be callers client handle.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated