Kernel Trace enabling/disabling/application interface.
This will have the definitions for kernel side traces statements and also details of variable traces supported in existing implementation.
#include <ti/syslink/utils/OsalPrint.h>
Go to the source code of this file.
Defines | |
#define | OSALTRACE_MODULEID (UInt16) 0xDA50 |
Module ID for OsalTrace OSAL module. | |
#define | GT_TRACESTATE_MASK 0x0000000F |
Trace state mask. | |
#define | GT_TRACESTATE_SHIFT 0u |
Bit shift for trace state. | |
#define | GT_TRACEENTER_MASK 0x000000F0 |
Trace enter mask. | |
#define | GT_TRACEENTER_SHIFT 4u |
Bit shift for trace enter. | |
#define | GT_TRACESETFAILURE_MASK 0x00000F00 |
Trace Set Failure Reason mask. | |
#define | GT_TRACESETFAILURE_SHIFT 8u |
Bit shift for trace Set Failure Reason. | |
#define | GT_TRACECLASS_MASK 0x000F0000 |
GT class mask. | |
#define | GT_TRACECLASS_SHIFT 16u |
Bit shift for GT class mask. | |
#define | GT_assert(x, y) |
#define | GT_setFailureReason(mask, classId, func, status, msg) |
#define | GT_0trace(mask, classId, format) |
#define | GT_1trace(mask, classId, format, arg1) |
#define | GT_2trace(mask, classId, format, arg1, arg2) |
#define | GT_3trace(mask, classId, format, arg1, arg2, arg3) |
#define | GT_4trace(mask, classId, format, arg1, arg2, arg3, arg4) |
#define | GT_5trace(mask, classId, format, arg1, arg2, arg3, arg4, arg5) |
#define | GT_setTrace(mask, type) 0 |
Enumerations | |
enum | GT_TraceState { GT_TraceState_Disable = 0x00000000, GT_TraceState_Enable = 0x00000001, GT_TraceState_EndValue = 0x00000002 } |
Enumerates the types of states of trace (enable/disable) More... | |
enum | GT_TraceEnter { GT_TraceEnter_Disable = 0x00000000, GT_TraceEnter_Enable = 0x00000010, GT_TraceEnter_EndValue = 0x00000020 } |
Enumerates the states of enter/leave trace (enable/disable) More... | |
enum | GT_TraceSetFailure { GT_TraceSetFailure_Disable = 0x00000000, GT_TraceSetFailure_Enable = 0x00000100, GT_TraceSetFailure_EndValue = 0x00000200 } |
Enumerates the states of SetFailureReason trace (enable/disable) More... | |
enum | GT_TraceClass { GT_1CLASS = 0x00010000, GT_2CLASS = 0x00020000, GT_3CLASS = 0x00030000, GT_4CLASS = 0x00040000, GT_ENTER = 0x00050000, GT_LEAVE = 0x00060000 } |
Enumerates the types of trace classes. More... | |
enum | GT_TraceType { GT_TraceType_User = 0x00000000, GT_TraceType_Kernel = 0x00000001, GT_TraceType_EndValue = 0x00000003 } |
Enumerates the types of trace. More... |
#define OSALTRACE_MODULEID (UInt16) 0xDA50 |
Module ID for OsalTrace OSAL module.
#define GT_TRACESTATE_MASK 0x0000000F |
Trace state mask.
#define GT_TRACESTATE_SHIFT 0u |
Bit shift for trace state.
#define GT_TRACEENTER_MASK 0x000000F0 |
Trace enter mask.
#define GT_TRACEENTER_SHIFT 4u |
Bit shift for trace enter.
#define GT_TRACESETFAILURE_MASK 0x00000F00 |
Trace Set Failure Reason mask.
#define GT_TRACESETFAILURE_SHIFT 8u |
Bit shift for trace Set Failure Reason.
#define GT_TRACECLASS_MASK 0x000F0000 |
GT class mask.
#define GT_TRACECLASS_SHIFT 16u |
Bit shift for GT class mask.
#define GT_assert | ( | x, | |
y | |||
) |
#define GT_setFailureReason | ( | mask, | |
classId, | |||
func, | |||
status, | |||
msg | |||
) |
#define GT_0trace | ( | mask, | |
classId, | |||
format | |||
) |
#define GT_1trace | ( | mask, | |
classId, | |||
format, | |||
arg1 | |||
) |
#define GT_2trace | ( | mask, | |
classId, | |||
format, | |||
arg1, | |||
arg2 | |||
) |
#define GT_3trace | ( | mask, | |
classId, | |||
format, | |||
arg1, | |||
arg2, | |||
arg3 | |||
) |
#define GT_4trace | ( | mask, | |
classId, | |||
format, | |||
arg1, | |||
arg2, | |||
arg3, | |||
arg4 | |||
) |
#define GT_5trace | ( | mask, | |
classId, | |||
format, | |||
arg1, | |||
arg2, | |||
arg3, | |||
arg4, | |||
arg5 | |||
) |
#define GT_setTrace | ( | mask, | |
type | |||
) | 0 |
enum GT_TraceState |
enum GT_TraceEnter |
enum GT_TraceSetFailure |
enum GT_TraceClass |
Enumerates the types of trace classes.
enum GT_TraceType |