Detailed Description
Header file implementing Memory manager . It is a wrapper implementation to support Shared memory allocation using heap address translations using shared region. or Tiler buffer allocation using tiler buffer manager and address translations.
Currently supports only shared Memory allocation using heap and shared region address translations.
Go to the source code of this file.
Data Structures |
struct | SyslinkMemMgr_CreateParams_tag |
| Structure defining common create parameters for the Memory manager module.Should be the first element in implementation specific create params. More...
|
struct | SyslinkMemMgr_freeParams_tag |
Defines |
#define | MEMMGR_MAX_NAME_LENGTH 32u |
#define | SyslinkMemMgr_Params SyslinkMemMgr_CreateParams |
Typedefs |
typedef enum
SyslinkMemMgr_Type_Type_tag | SyslinkMemMgr_Type |
| enum for denoting the different types of SyslinkMemMgr implementations.
|
typedef struct
SyslinkMemMgr_CreateParams_tag | SyslinkMemMgr_CreateParams |
| Structure defining common create parameters for the Memory manager module.Should be the first element in implementation specific create params.
|
typedef struct
SyslinkMemMgr_freeParams_tag | SyslinkMemMgr_freeParams |
typedef struct SyslinkMemMgr_Object | SyslinkMemMgr_Object |
| Forward declaration of structure defining object for the MemoryManger.
|
typedef struct
SyslinkMemMgr_Object * | SyslinkMemMgr_Handle |
| Handle for the MemoryManager instance.
|
Enumerations |
enum | SyslinkMemMgr_AddrType {
SyslinkMemMgr_AddrType_Virtual = 0u,
SyslinkMemMgr_AddrType_Portable = 1u,
SyslinkMemMgr_AddrType_EndValue = 2u
} |
| Enumerations to indicate address types used for translation.
More...
|
enum | SyslinkMemMgr_Type_Type_tag {
SyslinkMemMgr_TYPE_SHAREDMEM = 0x0,
SyslinkMemMgr_TYPE_TILERMEM = 0x1
} |
| enum for denoting the different types of SyslinkMemMgr implementations.
More...
|
Functions |
Int32 | SyslinkMemMgr_setup (Void) |
Int32 | SyslinkMemMgr_destroy (Void) |
SyslinkMemMgr_Handle | SyslinkMemMgr_create (Ptr params) |
Int32 | SyslinkMemMgr_delete (SyslinkMemMgr_Handle *pHandle) |
Ptr | SyslinkMemMgr_alloc (SyslinkMemMgr_Handle handle, UInt32 size, UInt32 align) |
Int32 | SyslinkMemMgr_free (SyslinkMemMgr_Handle handle, Ptr ptr, UInt32 size) |
Ptr | SyslinkMemMgr_map (SyslinkMemMgr_Handle handle, Ptr arg) |
Int32 | SyslinkMemMgr_unmap (SyslinkMemMgr_Handle handle, Ptr arg) |
Ptr | SyslinkMemMgr_translate (SyslinkMemMgr_Handle handle, Ptr srcAddr, SyslinkMemMgr_AddrType srcAddrType, SyslinkMemMgr_AddrType desAddrType) |
Ptr | SyslinkMemMgr_getKnlHandle (SyslinkMemMgr_Handle handle) |
Define Documentation
#define MEMMGR_MAX_NAME_LENGTH 32u |
Typedef Documentation
enum for denoting the different types of SyslinkMemMgr implementations.
Structure defining common create parameters for the Memory manager module.Should be the first element in implementation specific create params.
Forward declaration of structure defining object for the MemoryManger.
Handle for the MemoryManager instance.
Enumeration Type Documentation
Enumerations to indicate address types used for translation.
- Enumerator:
SyslinkMemMgr_AddrType_Virtual |
Virtual address on calling process on DSP where MMU is not configured it could be physical address.
|
SyslinkMemMgr_AddrType_Portable |
This is the shared region address incase sharedmemory manager plugged in to frameQbufMgr. In case of tiler it could be the tiler specific portable address
|
SyslinkMemMgr_AddrType_EndValue |
End delimiter indicating start of invalid values for this enum
|
enum for denoting the different types of SyslinkMemMgr implementations.
- Enumerator:
SyslinkMemMgr_TYPE_SHAREDMEM |
|
SyslinkMemMgr_TYPE_TILERMEM |
|
Function Documentation