From RTSC-Pedia

Jump to: navigation, search
revision tip
—— LANDSCAPE orientation
[printable version]  [offline version]offline version generated on 11-Jun-2009 18:06 UTC

RTSC+Eclipse FAQs

Using RTSC with Eclipse-Based Tools


This page provides answers to frequently asked questions about using RTSC within an Eclipse IDE such as CCStudio v4.

Contents

Installation and setup issues

FAQ-080729-1 How can I change the version of XDCtools used to build an existing Eclipse project?
FAQ-080729-2 How can I change the version of XDCtools used to build new Eclipse projects?
FAQ-080730-2 How can I change the version of XDCtools used to control the Eclipse plug-ins?
FAQ-080729-4 How can I set my XDCPATH in an Eclipse IDE?

Creating a project

FAQ-080729-5 How can I share a configuration between Eclipse IDE projects?

Building the project

FAQ-080729-8 Where can I get help on troubleshooting build and runtime errors?
FAQ-080730-1 How can I resolve linking issues with v6.1 of the C6000 compiler?

See also

RTSC+CCStudio v4 QuickStart Using CCStudio v4 to create, build, and debug RTSC projects
Runtime Object Viewer Using ROV for Eclipse-Based Debugging
Trouble Shooting Frequently encountered problems and their solutions

[printable version]  [offline version]offline version generated on 11-Jun-2009 18:06 UTC
Copyright © 2008 The Eclipse Foundation. All Rights Reserved
Views
Personal tools
package reference