TI-RTOS Drivers  tidrivers_cc32xx_2_16_01_13
Data Structures | Macros | Typedefs | Enumerations | Functions
UART.h File Reference

Detailed Description

UART driver interface.

============================================================================

The UART header file should be included in an application as follows:

Operation

The UART driver simplifies reading and writing to any of the UART peripherals on the board with multiple modes of operation and performance. These include blocking, non-blocking, and polling as well as text/binary mode, echo and return characters. The board's UART pins must be configured before initializing the UART driver. The application initializes the UART driver by calling UART_init() and is then ready to open a UART by calling UART_open(), passing in a UART parameters data structure.

The APIs in this driver serve as an interface to a typical TI-RTOS application. The specific peripheral implementations are responsible to create all the SYS/BIOS specific primitives to allow for thread-safe operation.

Opening the driver

UART_Handle handle;
UART_Params params;
params.baudRate = someNewBaudRate;
handle = UART_open(someUART_configIndexValue, &params);
if (!handle) {
System_printf("UART did not open");
}

Writing data

const unsigned char hello[] = "Hello World\n";
ret = UART_write(handle, hello, sizeof(hello));
System_printf("The UART wrote %d bytes\n", ret);

Reading data

unsigned char rxBuffer[20];
ret = UART_read(handle, rxBuffer, sizeof(rxBuffer));
System_printf("The UART read %d bytes\n", ret);

Implementation

This module serves as the main interface for TI-RTOS applications. Its purpose is to redirect the module's APIs to specific peripheral implementations which are specified using a pointer to a UART_FxnTable.

The UART driver interface module is joined (at link time) to a NULL-terminated array of UART_Config data structures named UART_config. UART_config is implemented in the application with each entry being an instance of a UART peripheral. Each entry in UART_config contains a:

Stack requirements

It is STRONGLY discouraged to perform UART_read() or UART_write calls within the driver's own callback function when in UART_MODE_CALLBACK. Doing so will incur additional task or system stack size requirements. See the peripheral implementations' documentation for stack size estimations. It is expected that the user perform his/her own stack and usage analysis when choosing to nest these calls.

Instrumentation

The UART driver interface produces log statements if instrumentation is enabled.

Diagnostics Mask Log details
Diags_USER1 basic operations performed
Diags_USER2 detailed operations performed

#include <stdint.h>
#include <stddef.h>
Include dependency graph for UART.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  UART_Params
 UART Parameters. More...
 
struct  UART_FxnTable
 The definition of a UART function table that contains the required set of functions to control a specific UART driver implementation. More...
 
struct  UART_Config
 UART Global configuration. More...
 

Macros

#define UART_CMD_RESERVED   32
 
#define UART_STATUS_RESERVED   -32
 
#define UART_STATUS_SUCCESS   0
 Successful status code returned by UART_control(). More...
 
#define UART_STATUS_ERROR   -1
 Generic error status code returned by UART_control(). More...
 
#define UART_STATUS_UNDEFINEDCMD   -2
 An error status code returned by UART_control() for undefined command codes. More...
 
#define UART_CMD_PEEK   0
 Command code used by UART_control() to read the next unsigned char. More...
 
#define UART_CMD_ISAVAILABLE   1
 Command code used by UART_control() to determine if the read buffer is empty. More...
 
#define UART_CMD_GETRXCOUNT   2
 Command code used by UART_control() to determine how many unsigned chars are in the read buffer. More...
 
#define UART_CMD_RXENABLE   3
 Command code used by UART_control() to enable data receive by the UART. More...
 
#define UART_CMD_RXDISABLE   4
 Command code used by UART_control() to disable data received by the UART. More...
 
#define UART_ERROR   UART_STATUS_ERROR
 
#define UART_WAIT_FOREVER   (~0)
 Wait forever define. More...
 

Typedefs

typedef struct UART_ConfigUART_Handle
 A handle that is returned from a UART_open() call. More...
 
typedef void(* UART_Callback) (UART_Handle, void *buf, size_t count)
 The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The callback can occur in task or HWI context. More...
 
typedef enum UART_Mode UART_Mode
 UART mode settings. More...
 
typedef enum UART_ReturnMode UART_ReturnMode
 UART return mode settings. More...
 
typedef enum UART_DataMode UART_DataMode
 UART data mode settings. More...
 
typedef enum UART_Echo UART_Echo
 UART echo settings. More...
 
typedef enum UART_LEN UART_LEN
 UART data length settings. More...
 
typedef enum UART_STOP UART_STOP
 UART stop bit settings. More...
 
typedef enum UART_PAR UART_PAR
 UART parity type settings. More...
 
typedef struct UART_Params UART_Params
 UART Parameters. More...
 
typedef void(* UART_CloseFxn) (UART_Handle handle)
 A function pointer to a driver specific implementation of UART_CloseFxn(). More...
 
typedef int(* UART_ControlFxn) (UART_Handle handle, unsigned int cmd, void *arg)
 A function pointer to a driver specific implementation of UART_ControlFxn(). More...
 
typedef void(* UART_InitFxn) (UART_Handle handle)
 A function pointer to a driver specific implementation of UART_InitFxn(). More...
 
typedef UART_Handle(* UART_OpenFxn) (UART_Handle handle, UART_Params *params)
 A function pointer to a driver specific implementation of UART_OpenFxn(). More...
 
typedef int(* UART_ReadFxn) (UART_Handle handle, void *buffer, size_t size)
 A function pointer to a driver specific implementation of UART_ReadFxn(). More...
 
typedef int(* UART_ReadPollingFxn) (UART_Handle handle, void *buffer, size_t size)
 A function pointer to a driver specific implementation of UART_ReadPollingFxn(). More...
 
typedef void(* UART_ReadCancelFxn) (UART_Handle handle)
 A function pointer to a driver specific implementation of UART_ReadCancelFxn(). More...
 
typedef int(* UART_WriteFxn) (UART_Handle handle, const void *buffer, size_t size)
 A function pointer to a driver specific implementation of UART_WriteFxn(). More...
 
typedef int(* UART_WritePollingFxn) (UART_Handle handle, const void *buffer, size_t size)
 A function pointer to a driver specific implementation of UART_WritePollingFxn(). More...
 
typedef void(* UART_WriteCancelFxn) (UART_Handle handle)
 A function pointer to a driver specific implementation of UART_WriteCancelFxn(). More...
 
typedef struct UART_FxnTable UART_FxnTable
 The definition of a UART function table that contains the required set of functions to control a specific UART driver implementation. More...
 
typedef struct UART_Config UART_Config
 UART Global configuration. More...
 

Enumerations

enum  UART_Mode {
  UART_MODE_BLOCKING,
  UART_MODE_CALLBACK
}
 UART mode settings. More...
 
enum  UART_ReturnMode {
  UART_RETURN_FULL,
  UART_RETURN_NEWLINE
}
 UART return mode settings. More...
 
enum  UART_DataMode {
  UART_DATA_BINARY = 0,
  UART_DATA_TEXT = 1
}
 UART data mode settings. More...
 
enum  UART_Echo {
  UART_ECHO_OFF = 0,
  UART_ECHO_ON = 1
}
 UART echo settings. More...
 
enum  UART_LEN {
  UART_LEN_5 = 0,
  UART_LEN_6 = 1,
  UART_LEN_7 = 2,
  UART_LEN_8 = 3
}
 UART data length settings. More...
 
enum  UART_STOP {
  UART_STOP_ONE = 0,
  UART_STOP_TWO = 1
}
 UART stop bit settings. More...
 
enum  UART_PAR {
  UART_PAR_NONE = 0,
  UART_PAR_EVEN = 1,
  UART_PAR_ODD = 2,
  UART_PAR_ZERO = 3,
  UART_PAR_ONE = 4
}
 UART parity type settings. More...
 

Functions

void UART_close (UART_Handle handle)
 Function to close a UART peripheral specified by the UART handle. More...
 
int UART_control (UART_Handle handle, unsigned int cmd, void *arg)
 Function performs implementation specific features on a given UART_Handle. More...
 
void UART_init (void)
 Function to initialize the UART module. More...
 
UART_Handle UART_open (unsigned int index, UART_Params *params)
 Function to initialize a given UART peripheral. More...
 
void UART_Params_init (UART_Params *params)
 Function to initialize the UART_Params struct to its defaults. More...
 
int UART_write (UART_Handle handle, const void *buffer, size_t size)
 Function that writes data to a UART with interrupts enabled. Usage of this API is mutually exclusive with usage of UART_writePolling(). In other words, for an opened UART peripheral, either UART_write() or UART_writePolling() may be used, but not both. More...
 
int UART_writePolling (UART_Handle handle, const void *buffer, size_t size)
 Function that writes data to a UART, polling the peripheral to wait until new data can be written. Usage of this API is mutually exclusive with usage of UART_write(). More...
 
void UART_writeCancel (UART_Handle handle)
 Function that cancels a UART_write() function call. More...
 
int UART_read (UART_Handle handle, void *buffer, size_t size)
 Function that reads data from a UART with interrupt enabled. This API must be used mutually exclusive with UART_readPolling(). More...
 
int UART_readPolling (UART_Handle handle, void *buffer, size_t size)
 Function that reads data from a UART without interrupts. This API must be used mutually exclusive with UART_read(). More...
 
void UART_readCancel (UART_Handle handle)
 Function that cancels a UART_read() function call. More...
 

Macro Definition Documentation

#define UART_ERROR   UART_STATUS_ERROR
#define UART_WAIT_FOREVER   (~0)

Wait forever define.

Typedef Documentation

typedef struct UART_Config* UART_Handle

A handle that is returned from a UART_open() call.

typedef void(* UART_Callback) (UART_Handle, void *buf, size_t count)

The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The callback can occur in task or HWI context.

Warning
Making UART_read() or UART_write() calls within its own callback routines are STRONGLY discouraged as it will impact Task and System stack size requirements! See the documentation for the specific driver implementations for additional estimated stack requirements.
Parameters
UART_HandleUART_Handle
bufPointer to read/write buffer
countNumber of elements read/written
typedef enum UART_Mode UART_Mode

UART mode settings.

This enum defines the read and write modes for the configured UART.

UART return mode settings.

This enumeration defines the return modes for UART_read() and UART_readPolling(). This mode only functions when in UART_DATA_TEXT mode.

UART_RETURN_FULL unblocks or performs a callback when the read buffer has been filled. UART_RETURN_NEWLINE unblocks or performs a callback whenever a newline character has been received.

UART operation UART_RETURN_FULL UART_RETURN_NEWLINE
UART_read Returns when buffer is full Returns when buffer is full or newline was read
UART_write Sends data as is Sends data with an additional newline at the end
Precondition
UART driver must be used in UART_DATA_TEXT mode.

UART data mode settings.

This enumeration defines the data mode for read and write. In UART_DATA_TEXT mode the driver will examine the UART_ReturnMode value.

typedef enum UART_Echo UART_Echo

UART echo settings.

This enumeration defines if the driver will echo data when uses in UART_DATA_TEXT mode. This only applies to data received by the UART.

UART_ECHO_ON will echo back characters it received while in UART_DATA_TEXT mode. UART_ECHO_OFF will not echo back characters it received in UART_DATA_TEXT mode.

Precondition
UART driver must be used in UART_DATA_TEXT mode.
typedef enum UART_LEN UART_LEN

UART data length settings.

This enumeration defines the UART data lengths.

typedef enum UART_STOP UART_STOP

UART stop bit settings.

This enumeration defines the UART stop bits.

typedef enum UART_PAR UART_PAR

UART parity type settings.

This enumeration defines the UART parity types.

typedef struct UART_Params UART_Params

UART Parameters.

UART parameters are used to with the UART_open() call. Default values for these parameters are set using UART_Params_init().

See also
UART_Params_init()
typedef void(* UART_CloseFxn) (UART_Handle handle)

A function pointer to a driver specific implementation of UART_CloseFxn().

typedef int(* UART_ControlFxn) (UART_Handle handle, unsigned int cmd, void *arg)

A function pointer to a driver specific implementation of UART_ControlFxn().

typedef void(* UART_InitFxn) (UART_Handle handle)

A function pointer to a driver specific implementation of UART_InitFxn().

typedef UART_Handle(* UART_OpenFxn) (UART_Handle handle, UART_Params *params)

A function pointer to a driver specific implementation of UART_OpenFxn().

typedef int(* UART_ReadFxn) (UART_Handle handle, void *buffer, size_t size)

A function pointer to a driver specific implementation of UART_ReadFxn().

typedef int(* UART_ReadPollingFxn) (UART_Handle handle, void *buffer, size_t size)

A function pointer to a driver specific implementation of UART_ReadPollingFxn().

typedef void(* UART_ReadCancelFxn) (UART_Handle handle)

A function pointer to a driver specific implementation of UART_ReadCancelFxn().

typedef int(* UART_WriteFxn) (UART_Handle handle, const void *buffer, size_t size)

A function pointer to a driver specific implementation of UART_WriteFxn().

typedef int(* UART_WritePollingFxn) (UART_Handle handle, const void *buffer, size_t size)

A function pointer to a driver specific implementation of UART_WritePollingFxn().

typedef void(* UART_WriteCancelFxn) (UART_Handle handle)

A function pointer to a driver specific implementation of UART_WriteCancelFxn().

typedef struct UART_FxnTable UART_FxnTable

The definition of a UART function table that contains the required set of functions to control a specific UART driver implementation.

typedef struct UART_Config UART_Config

UART Global configuration.

The UART_Config structure contains a set of pointers used to characterize the UART driver implementation.

This structure needs to be defined before calling UART_init() and it must not be changed thereafter.

See also
UART_init()

Enumeration Type Documentation

enum UART_Mode

UART mode settings.

This enum defines the read and write modes for the configured UART.

Enumerator
UART_MODE_BLOCKING 

Uses a semaphore to block while data is being sent. Context of the call must be a Task.

UART_MODE_CALLBACK 

Non-blocking and will return immediately. When UART_write() or UART_read() has finished, the callback function is called from either the caller's context or from an interrupt context.

UART return mode settings.

This enumeration defines the return modes for UART_read() and UART_readPolling(). This mode only functions when in UART_DATA_TEXT mode.

UART_RETURN_FULL unblocks or performs a callback when the read buffer has been filled. UART_RETURN_NEWLINE unblocks or performs a callback whenever a newline character has been received.

UART operation UART_RETURN_FULL UART_RETURN_NEWLINE
UART_read Returns when buffer is full Returns when buffer is full or newline was read
UART_write Sends data as is Sends data with an additional newline at the end
Precondition
UART driver must be used in UART_DATA_TEXT mode.
Enumerator
UART_RETURN_FULL 

Unblock/callback when buffer is full.

UART_RETURN_NEWLINE 

Unblock/callback when newline character is received.

UART data mode settings.

This enumeration defines the data mode for read and write. In UART_DATA_TEXT mode the driver will examine the UART_ReturnMode value.

Enumerator
UART_DATA_BINARY 

Data is not processed

UART_DATA_TEXT 

Data is processed according to above

enum UART_Echo

UART echo settings.

This enumeration defines if the driver will echo data when uses in UART_DATA_TEXT mode. This only applies to data received by the UART.

UART_ECHO_ON will echo back characters it received while in UART_DATA_TEXT mode. UART_ECHO_OFF will not echo back characters it received in UART_DATA_TEXT mode.

Precondition
UART driver must be used in UART_DATA_TEXT mode.
Enumerator
UART_ECHO_OFF 

Data is not echoed

UART_ECHO_ON 

Data is echoed

enum UART_LEN

UART data length settings.

This enumeration defines the UART data lengths.

Enumerator
UART_LEN_5 

Data length is 5 bits

UART_LEN_6 

Data length is 6 bits

UART_LEN_7 

Data length is 7 bits

UART_LEN_8 

Data length is 8 bits

enum UART_STOP

UART stop bit settings.

This enumeration defines the UART stop bits.

Enumerator
UART_STOP_ONE 

One stop bit

UART_STOP_TWO 

Two stop bits

enum UART_PAR

UART parity type settings.

This enumeration defines the UART parity types.

Enumerator
UART_PAR_NONE 

No parity

UART_PAR_EVEN 

Parity bit is even

UART_PAR_ODD 

Parity bit is odd

UART_PAR_ZERO 

Parity bit is always zero

UART_PAR_ONE 

Parity bit is always one

Function Documentation

void UART_close ( UART_Handle  handle)

Function to close a UART peripheral specified by the UART handle.

Precondition
UART_open() has been called.
Parameters
handleA UART_Handle returned from UART_open()
See also
UART_open()
int UART_control ( UART_Handle  handle,
unsigned int  cmd,
void *  arg 
)

Function performs implementation specific features on a given UART_Handle.

Commands for UART_control can originate from UART.h or from implementation specific UART*.h (UARTCC26XX.h, UARTTiva.h, etc.. ) files. While commands from UART.h are API portable across driver implementations, not all implementations may support all these commands. Conversely, commands from driver implementation specific UART*.h files add unique driver capabilities but are not API portable across all UART driver implementations.

Commands supported by UART.h follow a UART_CMD_<cmd> naming convention.
Commands supported by UART*.h follow a UART*_CMD_<cmd> naming convention.
Each control command defines arg differently. The types of arg are documented with each command.

See UART_control command codes for command codes.

See UART_control return status codes for status codes.

Precondition
UART_open() has to be called.
Parameters
handleA UART handle returned from UART_open()
cmdUART.h or UART*.h commands.
argAn optional R/W (read/write) command argument accompanied with cmd
Returns
Implementation specific return codes. Negative values indicate unsuccessful operations.
See also
UART_open()
void UART_init ( void  )

Function to initialize the UART module.

Precondition
The UART_config structure must exist and be persistent before this function can be called. This function must also be called before any other UART driver APIs.
UART_Handle UART_open ( unsigned int  index,
UART_Params params 
)

Function to initialize a given UART peripheral.

Function to initialize a given UART peripheral specified by the particular index value.

Precondition
UART_init() has been called
Parameters
indexLogical peripheral number for the UART indexed into the UART_config table
paramsPointer to a parameter block. If NULL, default parameter values will be used. All the fields in this structure are RO (read-only).
Returns
A UART_Handle upon success. NULL if an error occurs, or if the indexed UART peripheral is already opened.
See also
UART_init()
UART_close()
void UART_Params_init ( UART_Params params)

Function to initialize the UART_Params struct to its defaults.

Parameters
paramsAn pointer to UART_Params structure for initialization

Defaults values are: readMode = UART_MODE_BLOCKING; writeMode = UART_MODE_BLOCKING; readTimeout = UART_WAIT_FOREVER; writeTimeout = UART_WAIT_FOREVER; readCallback = NULL; writeCallback = NULL; readReturnMode = UART_RETURN_NEWLINE; readDataMode = UART_DATA_TEXT; writeDataMode = UART_DATA_TEXT; readEcho = UART_ECHO_ON; baudRate = 115200; dataLength = UART_LEN_8; stopBits = UART_STOP_ONE; parityType = UART_PAR_NONE;

int UART_write ( UART_Handle  handle,
const void *  buffer,
size_t  size 
)

Function that writes data to a UART with interrupts enabled. Usage of this API is mutually exclusive with usage of UART_writePolling(). In other words, for an opened UART peripheral, either UART_write() or UART_writePolling() may be used, but not both.

In UART_MODE_BLOCKING, UART_write() will block task execution until all the data in buffer has been written.

In UART_MODE_CALLBACK, UART_write() does not block task execution and calls a callback function specified by writeCallback. The callback function can occur in the caller's task context or in a HWI or SWI context, depending on the device.

Warning
It is STRONGLY discouraged to call UART_write from its own callback function (UART_MODE_CALLBACK).
See also
UART_writePolling()
Parameters
handleA UART_Handle
bufferA WO (write-only) pointer to buffer containing data to be written to the UART.
sizeThe number of bytes in the buffer that should be written to the UART.
Returns
Returns the number of bytes that have been written to the UART. If an error occurs, UART_ERROR is returned. In UART_MODE_CALLBACK, the return value is always 0.
int UART_writePolling ( UART_Handle  handle,
const void *  buffer,
size_t  size 
)

Function that writes data to a UART, polling the peripheral to wait until new data can be written. Usage of this API is mutually exclusive with usage of UART_write().

This function initiates an operation to write data to a UART controller.

UART_writePolling() will not return until all the data was written to the UART (or to its FIFO if applicable).

See also
UART_write()
Parameters
handleA UART_Handle
bufferA pointer to the buffer containing the data to be written to the UART.
sizeThe number of bytes in the buffer that should be written to the UART.
Returns
Returns the number of bytes that have been written to the UART. If an error occurs, UART_ERROR is returned.
void UART_writeCancel ( UART_Handle  handle)

Function that cancels a UART_write() function call.

This function cancels a UART_write() operation to a UART peripheral. This function is only applicable to UART_MODE_CALLBACK.

Parameters
handleA UART_Handle
int UART_read ( UART_Handle  handle,
void *  buffer,
size_t  size 
)

Function that reads data from a UART with interrupt enabled. This API must be used mutually exclusive with UART_readPolling().

This function initiates an operation to read data from a UART controller.

In UART_MODE_BLOCKING, UART_read() will block task execution until all the data in buffer has been read.

In UART_MODE_CALLBACK, UART_read does not block task execution an calls a callback function specified by readCallback. The callback function can occur in the caller's or in HWI or SWI context, depending on the device.

Warning
It is STRONGLY discouraged to call UART_read from its own callback function (UART_MODE_CALLBACK).
See also
UART_readPolling()
Parameters
handleA UART_Handle
bufferA RO (read-only) pointer to an empty buffer in which received data should be written to.
sizeThe number of bytes to be written into buffer
Returns
Returns the number of bytes that have been read from the UART, UART_ERROR on an error.
int UART_readPolling ( UART_Handle  handle,
void *  buffer,
size_t  size 
)

Function that reads data from a UART without interrupts. This API must be used mutually exclusive with UART_read().

This function initiates an operation to read data from a UART peripheral.

UART_readPolling will not return until size data was read to the UART.

See also
UART_read()
Parameters
handleA UART_Handle
bufferA RO (read-only) pointer to an empty buffer in which received data should be written to.
sizeThe number of bytes to be written into buffer
Returns
Returns the number of bytes that have been read from the UART, UART_ERROR on an error.
void UART_readCancel ( UART_Handle  handle)

Function that cancels a UART_read() function call.

This function cancels a UART_read() operation for a UART peripheral. This function is only applicable to UART_MODE_CALLBACK.

Parameters
handleA UART_Handle
Copyright 2016, Texas Instruments Incorporated