TI-RTOS Drivers  tidrivers_cc32xx_2_16_01_13
Data Structures
Here are the data structures with brief descriptions:
 CCamera_ConfigCamera Global configuration
 CCamera_FxnTableThe definition of a Camera function table that contains the required set of functions to control a specific Camera driver implementation
 CCamera_ParamsCamera Parameters
 CCameraCC3200DMA_HWAttrsCameraCC3200DMA Hardware attributes
 CCameraCC3200DMA_ObjectCameraCC3200DMA Object
 CClockP_FreqHzFrequency-in-hertz struct
 CClockP_ParamsBasic ClockP Parameters
 CDIR
 Cdiskio_fxns
 CEMAC_ConfigEMAC Global configuration
 CEMAC_FxnTableEMAC Function table structure
 CFATFS
 CFIL
 CFILINFO
 CGPIOCC3200_ConfigGPIO device specific driver configuration structure
 CHwiP_ParamsBasic HwiP Parameters
 CI2C_ConfigI2C Global configuration
 CI2C_FxnTableThe definition of a I2C function table that contains the required set of functions to control a specific I2C driver implementation
 CI2C_ParamsI2C Parameters
 CI2C_TransactionI2C transaction
 CI2CCC3200_HWAttrsI2CCC3200 Hardware attributes
 CI2CCC3200_ObjectI2CCC3200 Object
 CI2S_BufDescI2S buffer descriptor for issue/reclaim mode
 CI2S_ConfigI2S Global configuration
 CI2S_FxnTableThe definition of a I2S function table that contains the required set of functions to control a specific I2S driver implementation
 CI2S_ParamsBasic I2S Parameters
 CI2SCC3200DMA_HWAttrsI2SCC3200DMA Hardware attributes
 CI2SCC3200DMA_ObjectI2SCC3200DMA Object
 CI2SCC3200DMA_SerialPinConfigCC3200 Serial Pin Configuration
 CI2SCC3200DMA_SerialPinParamsCC3200 specific I2S Parameters
 CI2SCC3200DMA_SerialPinVarsI2SCC3200DMA Serial pin variables
 CList_Elem
 CList_List
 CMutexP_ParamsBasic MutexP Parameters
 CNVS_AttrsNVS attributes
 CNVS_ConfigNVS Global configuration
 CNVS_FxnTableThe definition of an NVS function table that contains the required set of functions to control a specific NVS driver implementation
 CNVS_ParamsNVS Parameters
 CNVSCC3200_CmdSetCopyBlockArgsNVSCC3200 command structure for setting copy block
 CNVSCC3200_HWAttrsNVSCC3200 attributes
 CNVSCC3200_Object
 CPIN_State_sUnderlying data structure for type PIN_State
 CPower_NotifyObjPower notify object structure
 CPowerCC3200_ConfigPower global configuration
 CPowerCC3200_MCURegistersMCU core registers that need to be save on entering LPDS
 CPowerCC3200_ModuleStateInternal module state
 CPowerCC3200_NVICRegistersNVIC registers that need to be save on entering LPDS
 CPowerCC3200_SaveRegistersStruct of context registers to save on entering LPDS
 CPowerCC3200_WakeupFor wakeup from LPDS or shutdown configuration
 CPWM_ConfigPWM Global configuration
 CPWM_FxnTableThe definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation
 CPWM_ParamsPWM Parameters
 CPWMTimerCC3200_HWAttrsPWMTimerCC3200 Hardware attributes
 CPWMTimerCC3200_ObjectPWMTimerCC3200 Object
 CRingBuf_Object
 CSDSPI_ConfigSDSPI Global configuration
 CSDSPI_FxnTableThe definition of a SDSPI function table that contains the required set of functions to control a specific SDSPI driver implementation
 CSDSPI_ParamsSDSPI Parameters
 CSDSPICC3200_HWAttrsSDSPICC3200 Hardware attributes
 CSDSPICC3200_ObjectSDSPICC3200 Object
 CSemaphoreP_ParamsBasic SemaphoreP Parameters
 CSPI_ConfigSPI Global configuration
 CSPI_FxnTableThe definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation
 CSPI_ParamsSPI Parameters
 CSPI_TransactionA SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK
 CSPICC3200DMA_HWAttrsSPICC3200DMA Hardware attributes
 CSPICC3200DMA_ObjectSPICC3200DMA Object
 CUART_ConfigUART Global configuration
 CUART_FxnTableThe definition of a UART function table that contains the required set of functions to control a specific UART driver implementation
 CUART_ParamsUART Parameters
 CUARTCC3200_FxnSetComplement set of read functions to be used by the UART ISR and UARTCC3200_read(). Internal use only
 CUARTCC3200_HWAttrsUARTCC3200 Hardware attributes
 CUARTCC3200_ObjectUARTCC3200 Object
 CUARTCC3200DMA_HWAttrsUARTCC3200DMA Hardware attributes
 CUARTCC3200DMA_ObjectUARTCC3200DMA Object
 CUSBMSCHFatFs_ConfigUSBMSCHFatFs Global configuration
 CUSBMSCHFatFs_FxnTableThe definition of a USBMSCHFatFs function table that contains the required set of functions to control a specific USBMSCHFatFs driver implementation
 CUSBMSCHFatFs_ParamsUSBMSCHFatFs Parameters
 CWatchdog_ConfigWatchdog Global configuration
 CWatchdog_FxnTableThe definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation
 CWatchdog_ParamsWatchdog Parameters
 CWatchdogCC3200_HWAttrsWatchdog hardware attributes for CC3200
 CWatchdogCC3200_ObjectWatchdog Object for CC3200
 CWiFi_ConfigWiFi Global configuration
 CWiFi_FxnTableThe definition of a WiFi function table that contains the required set of functions to control a specific WiFi driver implementation
 CWiFi_ParamsWiFi Parameters
 CWiFiCC3200_HWAttrsWiFiCC3200 Hardware attributes
 CWiFiCC3200_ObjectWiFiCC3200 Object
Copyright 2016, Texas Instruments Incorporated